Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino code help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1185 views
  • Users 0 members are here
  • buttons
  • led
  • code
  • arduino
Related

Arduino code help.

e14 Contributor
e14 Contributor over 12 years ago

I'm in the middle of an arduino project and I need help with the push buttons I'm using.

 

I need to be able to push a button that tells the arduino to set the LED value to 1 but not have the LED light up,

I also need there to be another button that makes all the push buttons that HAVE BEEN PRESSED light up.

 

Any help with the code or any resources that can help me are very much appreciated!

 

If this is not possible please tell me!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    byte leds[10];

     

    void reset() {

         for(int led=0; led<10; led++) {

              leds[led] = 0;

              digitalWrite(led, LOW);

         }

    }

     

    void set(int led) {

         if(led < 10 && led >= 0) leds[led] = 1;

    }

     

    void enableleds() {

         for(int led=0; led<10; led++)

              if(leds[led] ==1) digitalWrite(led, HIGH);

    }

     

    when a button is pressed have it call set passing it's led number

    when the reset button is pressed have it call the reset function

    when the enable button is pressed call the enableleds function

     

    Message was edited by: William Main changed to use digitalWrite (instead of pin which is for a different MCU library)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    byte leds[10];

     

    void reset() {

         for(int led=0; led<10; led++) {

              leds[led] = 0;

              digitalWrite(led, LOW);

         }

    }

     

    void set(int led) {

         if(led < 10 && led >= 0) leds[led] = 1;

    }

     

    void enableleds() {

         for(int led=0; led<10; led++)

              if(leds[led] ==1) digitalWrite(led, HIGH);

    }

     

    when a button is pressed have it call set passing it's led number

    when the reset button is pressed have it call the reset function

    when the enable button is pressed call the enableleds function

     

    Message was edited by: William Main changed to use digitalWrite (instead of pin which is for a different MCU library)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer