Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino code help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1190 views
  • Users 0 members are here
  • buttons
  • led
  • code
  • arduino
Related

Arduino code help.

e14 Contributor
e14 Contributor over 12 years ago

I'm in the middle of an arduino project and I need help with the push buttons I'm using.

 

I need to be able to push a button that tells the arduino to set the LED value to 1 but not have the LED light up,

I also need there to be another button that makes all the push buttons that HAVE BEEN PRESSED light up.

 

Any help with the code or any resources that can help me are very much appreciated!

 

If this is not possible please tell me!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    The idea is to have a project box with about 10 buttons on the project box and little LEDs next to them, wherever the LEDs are placed, there will be pieces of paper indicating what each button represents…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Just a note that to light 10 LEDs and monitor 12 switches is going to quickly outstrip your number of input/output pins on a basic arduino UNO. I would recommend using a few I2C chips (MCP23017) http://ww1.microchip.com/downloads/en/devicedoc/21952b.pdf. Up to 8 of these can be added to the same 2 wire bus. Each will provide 16 input/output bits. This would allow you 16 X 8 = 128 bits you can connect to for either input (button) or output (led). You can purchase a breakout with one chip from spikenzielabs.com. It is sold as I2C LCD Interface but can be used for any purpose.

     

    See the wire http://arduino.cc/en/Reference/Wire library.

     

    spikenzie labs sell just the mcp23017 chip for $1.89 each http://www.spikenzielabs.com/Catalog/index.php?main_page=product_info&cPath=2_30&products_id=16

     

    If you decide to go with the MCP23017, there is a library for the arduino here https://github.com/adafruit/Adafruit-MCP23017-Arduino-Library

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Just a note that to light 10 LEDs and monitor 12 switches is going to quickly outstrip your number of input/output pins on a basic arduino UNO. I would recommend using a few I2C chips (MCP23017) http://ww1.microchip.com/downloads/en/devicedoc/21952b.pdf. Up to 8 of these can be added to the same 2 wire bus. Each will provide 16 input/output bits. This would allow you 16 X 8 = 128 bits you can connect to for either input (button) or output (led). You can purchase a breakout with one chip from spikenzielabs.com. It is sold as I2C LCD Interface but can be used for any purpose.

     

    See the wire http://arduino.cc/en/Reference/Wire library.

     

    spikenzie labs sell just the mcp23017 chip for $1.89 each http://www.spikenzielabs.com/Catalog/index.php?main_page=product_info&cPath=2_30&products_id=16

     

    If you decide to go with the MCP23017, there is a library for the arduino here https://github.com/adafruit/Adafruit-MCP23017-Arduino-Library