Arduino
  • Products
  • More
Arduino
Arduino Forum Drive a 3d printer with "pure" arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 418 subscribers
  • Views 627 views
  • Users 0 members are here
Related

Drive a 3d printer with "pure" arduino?

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

One of my members has a question:

"Does anyone out there have any experience with driving a 3d printer using "standard" arduino, rather than the specialized boards usually used (RAMPS, sanguino, etc)?

thanks,"

His original request is here:

http://www.engineerslooking.com/need-stuff/drive-a-3d-printer-with-pure-arduino

  • Sign in to reply
  • Cancel
  • R_Phoenix
    0 R_Phoenix over 12 years ago

    Not sure why you would want to, what's the point?

    You will still need to use stepper motor drivers, relay shields to drive the hot end and build plate.

     

    To me, a RAMBO is a standard Arduino - it just has all the shields needed built onto the board. It is programmed in the Arduino IDE.

     

    Using an Arduino MEGA with shield after shield stacked on it with jumper going all over the place to me is a huge waste of time and effort.

     

    But - if you really want to, I believe the CupCake might be a place to start. If I remember correctly it started out with just an arduino Uno or MEGE driving it, or you migh find more info here
    http://reprap.org/wiki/RepRap

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello

     

    I think there is a confusion

    RAMPS is only an arduino shield which includes several interfaces

         - stepper motor interface

         - Extruder and bed heating power control

         - Min and Max travel switches

         - ...

    but an additional "pure" arduino board is needed (Arduino MEGA) to manage the 3D printer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nate1616
    0 Nate1616 over 12 years ago

    Hey Richard

    As most 3D printers use some form of a stepper motor you would need some form of a driver.  The purpose of the driver is to receive the pulses from the controller (example Adruino Mega) interpret its magnitude and then determines how and when the windings should be energized.  The driver also allows you to send larger voltages to get higher step rates than what the motor can handle by being a current limiter.  The last thing is that a standard arduino can not provide enough power for the motors.  Hope this clarifies this a little more

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer