Arduino
  • Products
  • More
Arduino
Arduino Forum Need help with multiple sound sensors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 416 subscribers
  • Views 420 views
  • Users 0 members are here
Related

Need help with multiple sound sensors

e14 Contributor
e14 Contributor over 12 years ago

So I'm trying to make a sound following robot, but I'm getting weird readings from my sensors...

 

I'm using a DFRobotShop Rover, NOT an UNO, I just couldnt find a good picture of the rover from above.

 

- DFRobotshop Rover with a duemilanove controller

- Two zxsound inex sound sensors

 

The sound sensors are supposed to just work with the 5v signal. It works perfectly if I try to use only one sensor, but messes up once I hook up the other sensor

 

This is my first post here so I'm sorry if the format is incorrect.

 

My code:

 

int Multiplier = 8;

int AnalogMax = 1023;

 

void setup() {

pinMode(5, OUTPUT);

pinMode(6, OUTPUT);

pinMode(7, OUTPUT);

pinMode(8, OUTPUT);

 

 

Serial.begin(9600);

 

}

 

void loop() {

 

int LeftEarBeta = analogRead(A2);

int RightEarBeta = analogRead(A3);

int LeftEar = (LeftEarBeta*Multiplier);

int RightEar = (RightEarBeta*Multiplier);

 

if(LeftEar>AnalogMax){

LeftEar=AnalogMax;

}

if(RightEar>AnalogMax){

RightEar=AnalogMax;

}

Serial.print(LeftEar);

Serial.print("        ");

Serial.println(RightEar); 

digitalWrite(7, HIGH);

digitalWrite(8, HIGH);

  analogWrite(5, LeftEar);

  analogWrite(6, RightEar);

  delay(20);

 

}

 

 

 

The multiplier int is just to make the motors more sensitive, but even if I set it at 1, the left mic is still picking up a constant signal of around 280?

What have I done wrong?

Attachments:
image
image
  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago

    The circuit of the sound sensors is truly horrible - they appear to be using some undocumented non linear characteristic of the amplifier driving  a huge capacitive load as a rectifier - you will never get good results from this.

     

    Despite that it doesn't explain why the two are so different - in your cicruit you have 10k resistors in series with the sound sensors power supplies - I don't think that is a good idea. They look as if they are intended to work connected directly to the supply.

     

    When you use just one sensor did you have the 10k resistor ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    When I hook up just one, it works fine, with or without the resistor. Should I just get a different brand of sound sensors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Look up the adafruit tutorial on their ampli-tie project.  They use their sound sensor(electret mic amp board) as input for a color organ.  If you look at the code, they sample the sound readings to account for noise and get a peak reading.  I built that project and there is a lot of electrical noise and you do have to adjust the mic sensitivity to get a useable range of readings.  The coding you use may have to be more sophisticated to smooth the input and multiples of sound sensors may just send things into a frenzy.  Maybe put an array of drinking straws in front of your mic element to simulate a "shotgun" mic to reduce the ambient noise.  Good luck.