Arduino
  • Products
  • More
Arduino
Arduino Forum Dc motor problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 418 subscribers
  • Views 1908 views
  • Users 0 members are here
Related

Dc motor problem

e14 Contributor
e14 Contributor over 12 years ago

Hi all just started with programming an Arduino UNO - I have no previous programming background!!

 

I started with Evil Genius book and I want to make a table feed for my milling machine, but right now im just experimenting with dc motor control.

 

What I have set up is a H Bridge (HMD-02)  2 buttons and 2 potentiometers and 1 dc motor

What i want it to do is 1 Nothing until I press 1 button then Turn forward at speed set by pot 1  , stop when i let go of button and turn backward at speed set by pot 2 when I press button 2???

 

MY sketch starts the motor running as soon as I compile and I cant find the problem??????

 

Please any help??

Many thanks.

Attachments:
dc_motor1.ino.zip
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks for the reply.  I was able to get it working and it was as you described.  I was also able to get a datasheet for the HMD-02A, all in Chinese, and with translation from a co-worker got the details.

     

    It turns out the 90A value is peak.  Constant is 40A.  It will handle motors from 3-25V and a PWM rate from 0-40kHz.  On the screw terminals, Out 1 and 2 are the motor, Vcc and Gnd are the motor power supply.  The other connector +5V and Gnd are for the circuit power.  In1 and 2 set the direction.  En is an enable pin, that's the one you wiggle with PWM.

     

    Here is the action of the pins:

     

    In1 hi In2 lo PWM active = CW motor

    In1 lo In2 Hi PWM active = CCW motor

    In1 lo In2 Lo PWM Hi = Motor Braking

    In1 don't care In2 don't care PWM Lo = motor off.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks for the reply.  I was able to get it working and it was as you described.  I was also able to get a datasheet for the HMD-02A, all in Chinese, and with translation from a co-worker got the details.

     

    It turns out the 90A value is peak.  Constant is 40A.  It will handle motors from 3-25V and a PWM rate from 0-40kHz.  On the screw terminals, Out 1 and 2 are the motor, Vcc and Gnd are the motor power supply.  The other connector +5V and Gnd are for the circuit power.  In1 and 2 set the direction.  En is an enable pin, that's the one you wiggle with PWM.

     

    Here is the action of the pins:

     

    In1 hi In2 lo PWM active = CW motor

    In1 lo In2 Hi PWM active = CCW motor

    In1 lo In2 Lo PWM Hi = Motor Braking

    In1 don't care In2 don't care PWM Lo = motor off.