Arduino
  • Products
  • More
Arduino
Arduino Forum Dc motor problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 418 subscribers
  • Views 1904 views
  • Users 0 members are here
Related

Dc motor problem

e14 Contributor
e14 Contributor over 12 years ago

Hi all just started with programming an Arduino UNO - I have no previous programming background!!

 

I started with Evil Genius book and I want to make a table feed for my milling machine, but right now im just experimenting with dc motor control.

 

What I have set up is a H Bridge (HMD-02)  2 buttons and 2 potentiometers and 1 dc motor

What i want it to do is 1 Nothing until I press 1 button then Turn forward at speed set by pot 1  , stop when i let go of button and turn backward at speed set by pot 2 when I press button 2???

 

MY sketch starts the motor running as soon as I compile and I cant find the problem??????

 

Please any help??

Many thanks.

Attachments:
dc_motor1.ino.zip
  • Sign in to reply
  • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to e14 Contributor

    Hello Gerhard,

     

    Thanks for the feedback. It was so obvious we all overlooked image you have to call the DigitalRead on a pin to get the value.

     

    Greetings,

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to vsluiter

    you have to call the DigitalRead on a pin to get the value.

    and unfortunately, there is no type checking to alert you to such a common mistake.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    yes small things easy to miss.

     

    This is why I plan to figure the code in small pieces then add the pieces together.

    1motor controll then add the LCD screen and then set limit switches then figure out how to have different modes!

     

    In a couple of YEARS I'll have a table feed for my mill.!

     

    Gerhard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I just bought one of these HMD-02 H-Bridge boards but mine did not come with any documentation.  The ebay seller hasn't gotten back to my request for information.

     

    I have some screw terminals labeled out1, Vcc,GND, out2.

     

    I also have some pins labeled +5,gnd,in1, in2, en.

     

    I need to speed control a single motor, don't need reversing.

     

    Does anyone have a pointer to a datasheet or wiring diagram for it?

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    I would imagine the motor will go across Out 1 and 2, supply for the motor to the + and - in between these pins

     

    Arduino output pins would go to in1 and in2, 5V and Gnd from Arduino to respective pins on that connector

     

    Educated guess on funtionality:

     

    0 on both in1 and 2, motor stationary, same if 1 (High) is set on those two pins

     

    if in 1 and 2 are different then the motor will turn one way or the other

     

    you should be able to test this without a motor connected by simply putting a meter on the out 1 and gnd or out 2 and gnd, change the input state and you should see the outputs change appropriately

     

    if you want to control only a simple dc motor then you could use this board to run two motors, one between out1 and gnd, one between out2 and gnd, you will loose direction control thats all.

     

    if you use a PWM output from Arduino you should be able to vary the speed of either side. If you have a motor across the outouts (Reversible) then only apply PWM to one side

     

    let me know how it goes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to Robert Peter Oakes

    btw, be warned, this is an educated guess, I do not have a circuit or a board to have tried this with

     

    It is how I would connect it if I did have one though, I take no responsibility for any outcome (Except Success image )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks for the reply.  I was able to get it working and it was as you described.  I was also able to get a datasheet for the HMD-02A, all in Chinese, and with translation from a co-worker got the details.

     

    It turns out the 90A value is peak.  Constant is 40A.  It will handle motors from 3-25V and a PWM rate from 0-40kHz.  On the screw terminals, Out 1 and 2 are the motor, Vcc and Gnd are the motor power supply.  The other connector +5V and Gnd are for the circuit power.  In1 and 2 set the direction.  En is an enable pin, that's the one you wiggle with PWM.

     

    Here is the action of the pins:

     

    In1 hi In2 lo PWM active = CW motor

    In1 lo In2 Hi PWM active = CCW motor

    In1 lo In2 Lo PWM Hi = Motor Braking

    In1 don't care In2 don't care PWM Lo = motor off.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<