Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Power Supply + Breadboards
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1751 views
  • Users 0 members are here
Related

Arduino Power Supply + Breadboards

hobbit666
hobbit666 over 12 years ago

I'm going to purchase a Arduino Starter kit soon to start playing with it.  I've watched a few youtube tutorials and Jeremy Blum stuff and like what it can do.

 

I dont have any sepcific projects in mind yet but on a few they talk about having seperate power supplies/rails other than the arduino 5V.  I'm planning at the moment of using just breadboards to play so will one of these (http://www.ebay.co.uk/itm/Breadboard-Power-Supply-for-Arduino-PIC-MB102-Dual-Output-BLACK-WINGS-/321058288624?pt=UK_BOI_Electrical_Test_Measurement_Equipment_ET&var=&hash=item4ac090b3f0) give me the seperate supply or LCD's/Motors/Relays etc?

 

If i wanted to create a prototype PCB would i then use a single power supply that has a Voltage and AMP rating big enough for the Microcontroller and motors/other things and use a seperate circuit to 'split' into different supplies as such?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you want to get a cheap power supply that will power an Uno and most shields (motors and LED strips, for example, take a lot more current/higher voltage) look at http://www.ebay.co.uk/itm/9-VOLT-9V-DC-MAINS-POWER-SUPPLY-ADAPTER-1000MA-ADAPTOR-/400230499907?pt=UK_Sound_Vision_Other&hash=item5d2f98c643 .

    A 9V adapter works great for Arduino, that adapter is 1A, so is plenty of current for most things, and the 2.5mm connector is the correct size for all Arduino boards (and Raspberry Pi, et al.).  Nothing magic about this particular adapter, other than with the specs I know it will work.  You can also use an old power adapter from some electronic device, that fits the specs.  Using a "breadboard power supply" is usually more trouble than it's worth when you're just starting off.  Having one you can plug into the wall and your Arduino's power port is much easier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you want to get a cheap power supply that will power an Uno and most shields (motors and LED strips, for example, take a lot more current/higher voltage) look at http://www.ebay.co.uk/itm/9-VOLT-9V-DC-MAINS-POWER-SUPPLY-ADAPTER-1000MA-ADAPTOR-/400230499907?pt=UK_Sound_Vision_Other&hash=item5d2f98c643 .

    A 9V adapter works great for Arduino, that adapter is 1A, so is plenty of current for most things, and the 2.5mm connector is the correct size for all Arduino boards (and Raspberry Pi, et al.).  Nothing magic about this particular adapter, other than with the specs I know it will work.  You can also use an old power adapter from some electronic device, that fits the specs.  Using a "breadboard power supply" is usually more trouble than it's worth when you're just starting off.  Having one you can plug into the wall and your Arduino's power port is much easier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • hobbit666
    0 hobbit666 over 12 years ago in reply to e14 Contributor

    So using that adaptor i would use the Uno 5V rail to power any electronics?

     

    Thanks for the advice.