Arduino
  • Products
  • More
Arduino
Arduino Forum Wireless temperature sensor help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 555 views
  • Users 0 members are here
  • help
  • wireless
  • arduino
  • sensor
  • question
Related

Wireless temperature sensor help.

funinalaska
funinalaska over 12 years ago

I Am looking for a way to build a temperature sensor network wirelessly.

I Would like to build a system to transmit data from a few DS18B20 and DHT11 or DHT22 sensors back to a central Arduino for display/log/web purposes. The initial idea will be using 2 wired sensors and 2 wireless sensors, but I would like it to be expandable for up to 8 wireless if I can.

how do I turn a digital sensor into a wireless module?

i Need are ware suggestions here.

I Am trying to keep cost low as well.

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    How to I turn a digital sensor into a wireless module depends on the wireless module you intend to use. If the wireless module has a digital input you could just connect the digital output from the sensor to the digital input of the wireless module. There also must be a way to determine from which sensor the data is. If the wireless module does not provide an ID, you must add identification to the data from the sensor. The sensor probably is providing continuous data. To be able to transmit the data this must be serial data.  If you just want to log room temperature and outside temperature one measurement per minute is more than sufficient. If the wireless transmitter-module contains a receiver, the central Arduino can ask the transmitter to transmit their message. Then with each sensor you need some control circuit that is listening to the central Arduino and will transmit its ID and data when asked for. If the wireless module can only transmit or receive analog signals like audio you need a simple modem to convert the digital signal into an audio signal. For instance the TCM3105. see http://www.tcm3105.com/tcm3105.pdf The first step is to select a wireless module and look at its specifications. Depending on the specifications of the wireless module you can make the interfaces to the  Arduino and the sensors. As a wireless module you could use a low power CB-radio. There are also digital thermometers for sale having a wireless outdoor sensor. Then you need to do some reverse engineering to get the data from the thermometer in your arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    How to I turn a digital sensor into a wireless module depends on the wireless module you intend to use. If the wireless module has a digital input you could just connect the digital output from the sensor to the digital input of the wireless module. There also must be a way to determine from which sensor the data is. If the wireless module does not provide an ID, you must add identification to the data from the sensor. The sensor probably is providing continuous data. To be able to transmit the data this must be serial data.  If you just want to log room temperature and outside temperature one measurement per minute is more than sufficient. If the wireless transmitter-module contains a receiver, the central Arduino can ask the transmitter to transmit their message. Then with each sensor you need some control circuit that is listening to the central Arduino and will transmit its ID and data when asked for. If the wireless module can only transmit or receive analog signals like audio you need a simple modem to convert the digital signal into an audio signal. For instance the TCM3105. see http://www.tcm3105.com/tcm3105.pdf The first step is to select a wireless module and look at its specifications. Depending on the specifications of the wireless module you can make the interfaces to the  Arduino and the sensors. As a wireless module you could use a low power CB-radio. There are also digital thermometers for sale having a wireless outdoor sensor. Then you need to do some reverse engineering to get the data from the thermometer in your arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer