Arduino
  • Products
  • More
Arduino
Arduino Forum MPG Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 442 views
  • Users 0 members are here
Related

MPG Arduino

e14 Contributor
e14 Contributor over 12 years ago

Want to make a MPG display using the Arduino. I will have a
Distance Pulse input and a Fuel Pulse input both will be 5vdc. I am faced with
the following conditions that I do not know how to do. Also I have other routine’s
that need to be run at the same time. I will have three outputs to an LCD,
current MPG, Trip MPG and an overall MPG.

 

  1. Need to read Distance & Fuel inputs in real
    time and store the readings as variables (cannot miss any pulses).
  2. Will need to store and read 4 or 5 variables that
    will NOT be reset or cleared when the Arduino is turned off. Whatever storage
    is suggested I want to be able send or read whole numbers and not have to break
    it down or read binary or Hex format.

 

Thanks for the help.

  • Sign in to reply
  • Cancel
Parents
  • kevjose
    0 kevjose over 12 years ago

    For the first application I would've used Interrupt pins on Arduino (Arduino Playground - Interrupts)

     

    As for storing data after the board is turned off. You could use EEPROMWrite (Arduino - EEPROMWrite) or you could attach an SD card to your setup to store values. I would suggest the former solution as you need to store only  very small amounts of data.

     

    This might be useful. Arduino Tutorial #13: Internal EEPROM - YouTube

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kevjose
    0 kevjose over 12 years ago

    For the first application I would've used Interrupt pins on Arduino (Arduino Playground - Interrupts)

     

    As for storing data after the board is turned off. You could use EEPROMWrite (Arduino - EEPROMWrite) or you could attach an SD card to your setup to store values. I would suggest the former solution as you need to store only  very small amounts of data.

     

    This might be useful. Arduino Tutorial #13: Internal EEPROM - YouTube