Arduino
  • Products
  • More
Arduino
Arduino Forum Help with a Arduino project Please
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 415 subscribers
  • Views 228 views
  • Users 0 members are here
Related

Help with a Arduino project Please

e14 Contributor
e14 Contributor over 12 years ago

Hi guys. I need your help with something. I’m a complete Newbie so please bear with me!

This is the scenario:

Amongst other non related hardware I have an 8ch relay module that I’ll be connecting to my Mega2560

To this is will connect 4 water pumps.

WP1

WP2

WP3

WP4

I want to run them in the following combinations, but it must select the flowDirection randomly and run it for 20mins

WP1 & WP4 = (flowDirection 1)

WP2 & WP3 = (flowDirection 2)

WP1 & WP2 = (flowDirection 3)

WP3 & WP4 = (flowDirection 4)

WP1 & WP3 = (flowDirection 5)

WP1 & WP3 = (flowDirection 6)

WP2 & WP4 = (flowDirection 7)

Then all the pumps must be off for 2 mins for the water settle/rest.

This will not be the only function I need the mega2560 to do so I don’t want the code to stop for 20mins every time this function starts!

Is this possible.

This is the code that I’ll also be running to run 4 channels LED that uses PWM for dimming.

// include the libraries:

#include <LiquidCrystal.h>

#include <Wire.h>

#include <Button.h>

#include <EEPROM.h>

#include <EEPROMVar.h>

 

 

/**** Define Variables & Constants ****/

/**************************************/

 

// set the RTC's I2C address

#define DS1307_I2C_ADDRESS 0x68

// create the LCD

LiquidCrystal lcd(8, 7, 5, 4, 16, 2);

// set up backlight

int bkl         = 6;        // backlight pin

byte bklIdle    = 10;       // PWM value for backlight at idle

byte bklOn      = 70;       // PWM value for backlight when on

int bklDelay    = 10000;    // ms for the backlight to idle before turning off

unsigned long bklTime = 0; // counter since backlight turned on

// create the menu counter

int menuCount   = 1;

int menuSelect = 0;

//create manual override variables

boolean override = false;

byte overmenu = 0;

int overpercent = 0;

// create the buttons

Button menu     = Button(12,PULLDOWN);

Button select   = Button(13,PULLDOWN);

Button plus     = Button(14,PULLDOWN);

Button minus    = Button(15,PULLDOWN);

 

// LED variables. These control the behavior of lighting. Change these to customize behavoir

int minCounter = 0; // counter that resets at midnight.

int oldMinCounter = 0; // counter that resets at midnight.

int oneLed = 9; // pin for channel 1

int twoLed = 10; // pin for channel 2

int threeLed = 11; // pin for channel 3

int fourLed = 3; // pin for channel 4

 

int oneVal = 0; // current value for channel 1

int twoVal = 0; // current value for channel 2

int threeVal = 0; // current value for channel 3

int fourVal = 0; // current value for channel 4

 

// Variables making use of EEPROM memory:

 

EEPROMVar<int> oneStartMins = 750;      // minute to start this channel.

EEPROMVar<int> onePhotoPeriod = 720;   // photoperiod in minutes for this channel.

EEPROMVar<int> oneMax = 100;           // max intensity for this channel, as a percentage

EEPROMVar<int> oneFadeDuration = 60;   // duration of the fade on and off for sunrise and sunset for

                                       //    this channel.

EEPROMVar<int> twoStartMins = 810;

EEPROMVar<int> twoPhotoPeriod = 600;

EEPROMVar<int> twoMax = 100;

EEPROMVar<int> twoFadeDuration = 60;

 

EEPROMVar<int> threeStartMins = 810;

EEPROMVar<int> threePhotoPeriod = 600;

EEPROMVar<int> threeMax = 100;

EEPROMVar<int> threeFadeDuration = 60;

 

EEPROMVar<int> fourStartMins = 480;

EEPROMVar<int> fourPhotoPeriod = 510; 

EEPROMVar<int> fourMax = 100;         

EEPROMVar<int> fourFadeDuration = 60; 

 

/*

int oneStartMins = 1380; // minute to start this channel.

int onePhotoPeriod = 120; // photoperiod in minutes for this channel.

int oneMax = 100; // max intensity for this channel, as a percentage

int oneFadeDuration = 60; // duration of the fade on and off for sunrise and sunset for

                                       //    this channel.                                   

int twoStartMins = 800;

int twoPhotoPeriod = 60;

int twoMax = 100;

int twoFadeDuration = 15;

 

int threeStartMins = 800;

int threePhotoPeriod = 60;

int threeMax = 100;

int threeFadeDuration = 30;

 

int fourStartMins = 800;

int fourPhotoPeriod = 120;

int fourMax = 100;

int fourFadeDuration = 60;

*/

 

/****** RTC Functions ******/

/***************************/

 

// Convert decimal numbers to binary coded decimal

byte decToBcd(byte val)

{

  return ( (val/10*16) + (val%10) );

}

 

// Convert binary coded decimal to decimal numbers

byte bcdToDec(byte val)

{

  return ( (val/16*10) + (val%16) );

}

 

// Sets date and time, starts the clock

void setDate(byte second,        // 0-59

             byte minute,        // 0-59

             byte hour,          // 1-23

             byte dayOfWeek,     // 1-7

             byte dayOfMonth,    // 1-31

             byte month,         // 1-12

             byte year)          // 0-99

{

Wire.beginTransmission(DS1307_I2C_ADDRESS);

   Wire.send(0);

Wire.send(decToBcd(second));

Wire.send(decToBcd(minute));

Wire.send(decToBcd(hour));

Wire.send(decToBcd(dayOfWeek));

Wire.send(decToBcd(dayOfMonth));

Wire.send(decToBcd(month));

Wire.send(decToBcd(year));

Wire.endTransmission();

}

 

// Gets the date and time

void getDate(byte *second,

             byte *minute,

             byte *hour,

             byte *dayOfWeek,

             byte *dayOfMonth,

             byte *month,

             byte *year)

{

Wire.beginTransmission(DS1307_I2C_ADDRESS);

  Wire.send(0);

Wire.endTransmission();

Wire.requestFrom(DS1307_I2C_ADDRESS, 7);

  *second     = bcdToDec(Wire.receive() & 0x7f);

  *minute     = bcdToDec(Wire.receive());

  *hour       = bcdToDec(Wire.receive() & 0x3f);

  *dayOfWeek  = bcdToDec(Wire.receive());

  *dayOfMonth = bcdToDec(Wire.receive());

  *month      = bcdToDec(Wire.receive());

  *year       = bcdToDec(Wire.receive());

}

 

/****** LED Functions ******/

/***************************/

//function to set LED brightness according to time of day

//function has three equal phases - ramp up, hold, and ramp down

 

int   setLed(int mins,    // current time in minutes

            int ledPin,  // pin for this channel of LEDs

            int start,   // start time for this channel of LEDs

            int period,  // photoperiod for this channel of LEDs

            int fade,    // fade duration for this channel of LEDs

            int ledMax   // max value for this channel

            )  {

  int val = 0;

     

      //fade up

      if (mins > start || mins <= start + fade)  {

        val = map(mins - start, 0, fade, 0, ledMax);

      }

      //fade down

      if (mins > start + period - fade && mins <= start + period)  {

        val = map(mins - (start + period - fade), 0, fade, ledMax, 0);

      }

      //off or post-midnight run.

      if (mins <= start || mins > start + period)  {

if((start+period)%1440 < start && (start + period)%1440 > mins )

          {

val=map((start+period-mins)%1440,0,fade,0,ledMax);

          }

        else 

        val = 0;

      }

   

   

    if (val > ledMax)  {val = ledMax;}

    if (val < 0) {val = 0; }

   

  analogWrite(ledPin, map(val, 0, 100, 0, 255));

  if(override){val=overpercent;}

  return val;

}

 

/**** Display Functions ****/

/***************************/

 

// format a number of minutes into a readable time (24 hr format)

void printMins(int mins,       //time in minutes to print

               boolean ampm    //print am/pm?

              )  {

  int hr = (mins%1440)/60;

  int mn = mins%60;

    if(hr<10){

      lcd.print(" ");

    }

    lcd.print(hr);

lcd.print(":");

    if(mn<10){

lcd.print("0");

    }

    lcd.print(mn);

}

 

// format hours, mins, secs into a readable time (24 hr format)

void printHMS (byte hr,

               byte mn,

               byte sec      //time to print

              ) 

{

 

    if(hr<10){

      lcd.print(" ");

    }

    lcd.print(hr, DEC);

    lcd.print(":");

    if(mn<10){

lcd.print("0");

    }

    lcd.print(mn, DEC);

    lcd.print(":");

    if(sec<10){

lcd.print("0");

    }

    lcd.print(sec, DEC);

}

void ovrSetAll(int pct){

analogWrite(oneLed,map(pct,0,100,0,255));

analogWrite(twoLed,map(pct,0,100,0,255));

analogWrite(threeLed,map(pct,0,100,0,255));

analogWrite(fourLed,map(pct,0,100,0,255));

}

 

/**** Setup ****/

/***************/

 

void setup() {

  Wire.begin();

  pinMode(bkl, OUTPUT);

  lcd.begin(16, 2);

  digitalWrite(bkl, HIGH);

lcd.print("Typhon-Reef");

  lcd.setCursor(0,1);

lcd.print("");

  delay(5000);

  lcd.clear();

analogWrite(bkl,bklIdle);

}

 

/***** Loop *****/

/****************/

 

void loop() {

  byte second, minute, hour, dayOfWeek, dayOfMonth, month, year;

 

  getDate(&second, &minute, &hour, &dayOfWeek, &dayOfMonth, &month, &year);

  oldMinCounter = minCounter;

  minCounter = hour * 60 + minute;

 

  //check & set fade durations

  if(oneFadeDuration > onePhotoPeriod/2 && onePhotoPeriod >0){oneFadeDuration = onePhotoPeriod/2;}

if(oneFadeDuration<1){oneFadeDuration=1;}

 

  if(twoFadeDuration > twoPhotoPeriod/2 && twoPhotoPeriod >0){twoFadeDuration = twoPhotoPeriod/2;}

  if(twoFadeDuration<1){twoFadeDuration=1;}

 

  if(threeFadeDuration > threePhotoPeriod/2 && threePhotoPeriod >0){threeFadeDuration = threePhotoPeriod/2;}

if(threeFadeDuration<1){threeFadeDuration=1;}

 

  if(fourFadeDuration > fourPhotoPeriod/2 && fourPhotoPeriod > 0){fourFadeDuration = fourPhotoPeriod/2;}

if(fourFadeDuration<1){fourFadeDuration=1;}

 

  //check & set any time functions

 

 

  //set outputs

  if(!override){

  oneVal = setLed(minCounter, oneLed, oneStartMins, onePhotoPeriod, oneFadeDuration, oneMax);

  twoVal = setLed(minCounter, twoLed, twoStartMins, twoPhotoPeriod, twoFadeDuration, twoMax);

  threeVal = setLed(minCounter, threeLed, threeStartMins, threePhotoPeriod, threeFadeDuration, threeMax);

  fourVal = setLed(minCounter, fourLed, fourStartMins, fourPhotoPeriod, fourFadeDuration, fourMax);

  }

  else{

ovrSetAll(overpercent);

  }