Arduino
  • Products
  • More
Arduino
Arduino Forum Switch anode current on with HIGH
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 679 views
  • Users 0 members are here
  • current
  • transistors
  • anode
Related

Switch anode current on with HIGH

e14 Contributor
e14 Contributor over 12 years ago

Hello. I hope the topic makes sense. I would like to add that this is for educational purposes, and that a dedicated driver IC would probably be better.

 

What I basically want to do is drive a multiplexed 4 digit common anode 7 segment, using some sort of current switching on the anode side and a shift register on the cathode side.

 

I have this circuit working with pnp transistors on the anode side (right on the schematic below). A low signal on pins 2,3,4 or 5 makes the current flow from the emitter to the collector, and the LED light up in the chosen digit (in a pattern controlled by the shift register).

 

Is there any way I can replace the PNP transistors with something that reacts the same way to a low signal? First thought was of course NPN transistors, but they have to go on the cathode side, which is not practical with this display. My plan is to try driving the anodes with a counter such as the CD4022 using the latch signal from the shift register, thus potentially saving 4 pins on my arduino.

image

(sorry about the messy schematic, it is a quick drawing for learning to work with the PCB-layouting tool in KiCAD)

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    You could wire four NPN transistors as emitter followers.  In this case the NPN collectors are connected to Vcc and the NPN bases are connected to your counter outputs.  You probably don't need resistors, since the current through the NPN base is limited by the amplification of the NPN transistor.  The emitters drive the common anodes for the four digits.

     

    An emitter follower does not pull up as high as your PNP transistors: it is limited to the high value of your counter output minus approx 0.7V drop across the NPN B-E junction.  However, if your counter outputs are near Vcc = 5V then pulling up to 4V is fine for the LEDs: just adjust the segment resistors.

     

    If your counter outputs don't pull up high enough by themselves, you can add additional pull-up resistors at the NPN bases.

     

    I don't think you're going to save all four pins -- you need one to synchronize the counter to a known state.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago

    You could wire four NPN transistors as emitter followers.  In this case the NPN collectors are connected to Vcc and the NPN bases are connected to your counter outputs.  You probably don't need resistors, since the current through the NPN base is limited by the amplification of the NPN transistor.  The emitters drive the common anodes for the four digits.

     

    An emitter follower does not pull up as high as your PNP transistors: it is limited to the high value of your counter output minus approx 0.7V drop across the NPN B-E junction.  However, if your counter outputs are near Vcc = 5V then pulling up to 4V is fine for the LEDs: just adjust the segment resistors.

     

    If your counter outputs don't pull up high enough by themselves, you can add additional pull-up resistors at the NPN bases.

     

    I don't think you're going to save all four pins -- you need one to synchronize the counter to a known state.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer