Arduino
  • Products
  • More
Arduino
Arduino Forum Switch anode current on with HIGH
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 677 views
  • Users 0 members are here
  • current
  • transistors
  • anode
Related

Switch anode current on with HIGH

e14 Contributor
e14 Contributor over 12 years ago

Hello. I hope the topic makes sense. I would like to add that this is for educational purposes, and that a dedicated driver IC would probably be better.

 

What I basically want to do is drive a multiplexed 4 digit common anode 7 segment, using some sort of current switching on the anode side and a shift register on the cathode side.

 

I have this circuit working with pnp transistors on the anode side (right on the schematic below). A low signal on pins 2,3,4 or 5 makes the current flow from the emitter to the collector, and the LED light up in the chosen digit (in a pattern controlled by the shift register).

 

Is there any way I can replace the PNP transistors with something that reacts the same way to a low signal? First thought was of course NPN transistors, but they have to go on the cathode side, which is not practical with this display. My plan is to try driving the anodes with a counter such as the CD4022 using the latch signal from the shift register, thus potentially saving 4 pins on my arduino.

image

(sorry about the messy schematic, it is a quick drawing for learning to work with the PCB-layouting tool in KiCAD)

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    Hi Niels,

    I'm not too clear exactly what the question is so I'll toss a couple of ideas to see if they apply...

    If you want to reduce component count, you could use FETs on the anodes to eliminate base resistors.

    If you want to change from active low to active high control signals you could use something like a PEMD6 or PUMD6 which can use an internal NPN transistor to invert the signal and drive the internal PNP transistor output. These parts even have the base resistors built-in. PUMD12 has even more resistors built-in. They cost about 39 cents.

    If you want to change from active low to active high control signals and consolidate 4 drivers into a single chip, you might try a quad op-amp such as an AD8534 which can source about 100 mA before the output sags 0.4 V. I don't know if .4 V will cause a noticeable difference in brightness, but it should be considered. Cost is just under $2.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago

    Hi Niels,

    I'm not too clear exactly what the question is so I'll toss a couple of ideas to see if they apply...

    If you want to reduce component count, you could use FETs on the anodes to eliminate base resistors.

    If you want to change from active low to active high control signals you could use something like a PEMD6 or PUMD6 which can use an internal NPN transistor to invert the signal and drive the internal PNP transistor output. These parts even have the base resistors built-in. PUMD12 has even more resistors built-in. They cost about 39 cents.

    If you want to change from active low to active high control signals and consolidate 4 drivers into a single chip, you might try a quad op-amp such as an AD8534 which can source about 100 mA before the output sags 0.4 V. I don't know if .4 V will cause a noticeable difference in brightness, but it should be considered. Cost is just under $2.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    I am sorry for not being clear. The specific question was meant to be changing active low to active high.

     

    The longer term goal was to reduce pin usage and possibly component count.

     

    The component count is not as important, but rather my goal is to use the stuff in my junk box (hence the counter, the 74hc595 shift register and the basic transistors).

     

    But a 12 bit shift register would certainly do the trick.