Arduino
  • Products
  • More
Arduino
Arduino Forum Switch anode current on with HIGH
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 679 views
  • Users 0 members are here
  • current
  • transistors
  • anode
Related

Switch anode current on with HIGH

e14 Contributor
e14 Contributor over 12 years ago

Hello. I hope the topic makes sense. I would like to add that this is for educational purposes, and that a dedicated driver IC would probably be better.

 

What I basically want to do is drive a multiplexed 4 digit common anode 7 segment, using some sort of current switching on the anode side and a shift register on the cathode side.

 

I have this circuit working with pnp transistors on the anode side (right on the schematic below). A low signal on pins 2,3,4 or 5 makes the current flow from the emitter to the collector, and the LED light up in the chosen digit (in a pattern controlled by the shift register).

 

Is there any way I can replace the PNP transistors with something that reacts the same way to a low signal? First thought was of course NPN transistors, but they have to go on the cathode side, which is not practical with this display. My plan is to try driving the anodes with a counter such as the CD4022 using the latch signal from the shift register, thus potentially saving 4 pins on my arduino.

image

(sorry about the messy schematic, it is a quick drawing for learning to work with the PCB-layouting tool in KiCAD)

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    Hi Niels,

    Another thought....

    Could you extend the shift register by 4 bits by cascading a second chip and use these to drive your PNP transistors? - no need for a Johnson counter, signal inversion or more Arduino pins - just make sure only one of the 4 "digit bits" is low.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 12 years ago

    Hi Niels,

    Another thought....

    Could you extend the shift register by 4 bits by cascading a second chip and use these to drive your PNP transistors? - no need for a Johnson counter, signal inversion or more Arduino pins - just make sure only one of the 4 "digit bits" is low.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer