Arduino
  • Products
  • More
Arduino
Arduino Forum Help with joining two pieces of code.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 45 replies
  • Subscribers 416 subscribers
  • Views 4126 views
  • Users 0 members are here
  • led
  • rgb
Related

Help with joining two pieces of code.

e14 Contributor
e14 Contributor over 12 years ago

Hey Arduino Family!

 

I got y first arduino this week and i havent put it down since it arrived, I'm totally hooked.

I'm really a complete novice with coding but I am slowly starting to take it on board and can somewhat understand what the lines of code are doing (even thought I never thought that I would! lol)

 

So I am making this kind ambient lamp from RGB leds

 

I have these two pieces of code that work just fine on their own.

One cycles through colours nicely in a rainbow kinda effect and the other allows the colours to be set using 3 pots that are controlling the PWM signal.

 

What I would like to do is connect a momentary push button switch that takes it out of the rainbow cycle code and places it into 'manual' mode handing over control to the user.

I was thinking that this would perhaps look something like this:

The main loop for the rainbow effect is running, at the top of the loop check to see if the button is pressed and if it is then exit the loop and continue down the program, at which point it would hit the next loop which is the manual control section, perhaps in this loop it could look for the button being pressed again and switch back to the first loop putting it back into rainbow mode again'

 

The two sketches I have been using are pasted below.

any help that will start pointing me in the right direction would be really appreciated. thanks guys. image

 

RGB Rainbow

const int redPin = 11;

const int greenPin = 10;

const int bluePin = 9;

 

void setup() {

  // Start off with the LED off.

  setColourRgb(0,0,0);

}

 

void loop() {

  unsigned int rgbColour[3];

 

  // Start off with red.

  rgbColour[0] = 255;

  rgbColour[1] = 0;

  rgbColour[2] = 0;

 

  // Choose the colours to increment and decrement.

  for (int decColour = 0; decColour < 3; decColour += 1) {

    int incColour = decColour == 2 ? 0 : decColour + 1;

 

    // cross-fade the two colours.

    for(int i = 0; i < 255; i += 1) {

      rgbColour[decColour] -= 1;

      rgbColour[incColour] += 1;

    

      setColourRgb(rgbColour[0], rgbColour[1], rgbColour[2]);

      delay(5);

    }

  }

}

 

void setColourRgb(unsigned int red, unsigned int green, unsigned int blue) {

  analogWrite(redPin, red);

  analogWrite(greenPin, green);

  analogWrite(bluePin, blue);

}

 

 

 

=================================================

 

RGB Color Chooser

 

// Init the Pins used for PWM

const int redPin = 9;

const int greenPin = 10;

const int bluePin = 11;

 

// Init the Pins used for 10K pots

const int redPotPin = 0;

const int greenPotPin = 1;

const int bluePotPin = 2;

 

// Init our Vars

int currentColorValueRed;

int currentColorValueGreen;

int currentColorValueBlue;

 

void setup()

{

  pinMode(redPin, OUTPUT);

  pinMode(greenPin, OUTPUT);

  pinMode(bluePin, OUTPUT);

}

 

void loop()

{

// Read the voltage on each analog pin then scale down to 0-255 and inverting the value for common anode

  currentColorValueRed = (255 - map( analogRead(redPotPin), 0, 1024, 0, 255 ) );

  currentColorValueBlue = (255 - map( analogRead(bluePotPin), 0, 1024, 0, 255 ) );

  currentColorValueGreen = (255 - map( analogRead(greenPotPin), 0, 1024, 0, 255 ) );

 

// Write the color to each pin using PWM and the value gathered above

  analogWrite(redPin, currentColorValueRed);

  analogWrite(bluePin, currentColorValueBlue);

  analogWrite(greenPin, currentColorValueGreen);

 

}

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Congratulations with the new board and your introduction to writing your own programs.  I am fairly new at this as well however.  I will give this one a shot.  I think an if... else statement would work perfectly here.  This function checks if an expression is true and executes a statement otherwise the else statement is executed.  I borrowed this bit of code from the great book "arduino cookbook" by Michael Margolis.

    /*

         Pushbutton Sketch

         a switch connecte to pin 2 lights the LED on pin 13

    */

    const int ledPin = 13;

    const in inputPin = 2;

     

    void setup () {

         pinMode(ledPin, OUTPUT);

         pinMode(inputPin, INPUT);

    }


    void loop(){

    int val = digitalRead(inputPin);

    if (val == HIGH)

    {

         digitalWrite(ledPin, HIGH);

    }

    else

    {

    digitalWrite(ledPin, LOW);

    }

    }


    in this example you are setting up the pin mode and telling the device what to do for each pin mode.  start your loop code with a { bracket then an if statement and then tell it what to do if that statement is true inside { }  otherwise the else statement will be used, the else statement is also inside { } brackets.. everything is wrapped up with a final closing }.

    Hope this helps. I had the same question for a telling the board to do one thing if a pin value was high and an other if it was low and this method worked for me.


    Of course your going to have to play with your pin assignments because each example sketch is using some of the same pins differently, for example in the first sketch pin 9 is blue but in the second example it is red.  good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Congratulations with the new board and your introduction to writing your own programs.  I am fairly new at this as well however.  I will give this one a shot.  I think an if... else statement would work perfectly here.  This function checks if an expression is true and executes a statement otherwise the else statement is executed.  I borrowed this bit of code from the great book "arduino cookbook" by Michael Margolis.

    /*

         Pushbutton Sketch

         a switch connecte to pin 2 lights the LED on pin 13

    */

    const int ledPin = 13;

    const in inputPin = 2;

     

    void setup () {

         pinMode(ledPin, OUTPUT);

         pinMode(inputPin, INPUT);

    }


    void loop(){

    int val = digitalRead(inputPin);

    if (val == HIGH)

    {

         digitalWrite(ledPin, HIGH);

    }

    else

    {

    digitalWrite(ledPin, LOW);

    }

    }


    in this example you are setting up the pin mode and telling the device what to do for each pin mode.  start your loop code with a { bracket then an if statement and then tell it what to do if that statement is true inside { }  otherwise the else statement will be used, the else statement is also inside { } brackets.. everything is wrapped up with a final closing }.

    Hope this helps. I had the same question for a telling the board to do one thing if a pin value was high and an other if it was low and this method worked for me.


    Of course your going to have to play with your pin assignments because each example sketch is using some of the same pins differently, for example in the first sketch pin 9 is blue but in the second example it is red.  good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    thanks chris,

    I just got up, going to check this out in a few minutes.

    appreciate the replies.