Arduino
  • Products
  • More
Arduino
Arduino Forum MP3 Player
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 415 subscribers
  • Views 316 views
  • Users 0 members are here
Related

MP3 Player

e14 Contributor
e14 Contributor over 12 years ago

I am trying to write a program to place a string in a funtion call, the function is ( boolean playFullFile(char *trackname) I am using an array to store int numbers I am renaming my MP3s 1 to 100 and would like to call them into function as *trackname. The program example is
musicPlayer.playFullFile("track001.mp3");.
Can you help me with this?

This is an example for the Adafruit VS1053 Codec Breakout

  Designed specifically to work with the Adafruit VS1053 Codec Breakout
  ----> https://www.adafruit.com/products/1381

  Adafruit invests time and resources providing this open source code,
  please support Adafruit and open-source hardware by purchasing
  products from Adafruit!

  Written by Limor Fried/Ladyada for Adafruit Industries. 
  BSD license, all text above must be included in any redistribution
****************************************************/

// include SPI, MP3 and SD libraries
#include <SPI.h>
#include <Adafruit_VS1053.h>
#include <SD.h>

// define the pins used
//#define CLK 13       // SPI Clock, shared with SD card
//#define MISO 12      // Input data, from VS1053/SD card
//#define MOSI 11      // Output data, to VS1053/SD card
// Connect CLK, MISO and MOSI to hardware SPI pins.
// See http://arduino.cc/en/Reference/SPI "Connections"

// These can be any pins:
#define RESET 9      // VS1053 reset pin (output)
#define CS 10        // VS1053 chip select pin (output)
#define DCS 8        // VS1053 Data/command select pin (output)
#define CARDCS 4     // Card chip select pin
// DREQ should be an Int pin, see http://arduino.cc/en/Reference/attachInterrupt
#define DREQ 3       // VS1053 Data request, ideally an Interrupt pin


Adafruit_VS1053_FilePlayer musicPlayer = Adafruit_VS1053_FilePlayer(RESET, CS, DCS, DREQ, CARDCS);

void setup() {
  Serial.begin(9600);
  Serial.println("Adafruit VS1053 Simple Test");

  musicPlayer.begin(); // initialise the music player
  SD.begin(CARDCS);    // initialise the SD card
 
  // Set volume for left, right channels. lower numbers == louder volume!
  musicPlayer.setVolume(20,20);

  musicPlayer.useInterrupt(VS1053_FILEPLAYER_TIMER0_INT); // timer int
  //musicPlayer.useInterrupt(VS1053_FILEPLAYER_PIN_INT);  // DREQ int
 
  // Play one file, don't return until complete
  musicPlayer.playFullFile("track001.mp3");
  // Play another file in the background, REQUIRES interrupts!
  musicPlayer.startPlayingFile("track002.mp3");
}

void loop() {
  // File is playing in the background
  if (! musicPlayer.playingMusic)
    Serial.println("Done playing music");
 
  delay(1000);
}