Arduino
  • Products
  • More
Arduino
Arduino Forum I was wondering if someone could look over this code?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 342 views
  • Users 0 members are here
  • arduino
Related

I was wondering if someone could look over this code?

e14 Contributor
e14 Contributor over 12 years ago

I want it to control a solenoid with an Arduino. If the correct pass key is entered of a valid finger is used, I want it to print on a LCD access granted, and unlock the door. If not, I want the LCD to say "Access Denied" and stay locked.  When their is nothing, I want it to say "Henry's Workroom", with the time displayed below. All the hardware, I'm pretty confident on, I'm using a Arduino Mega so don't worry about the abundance of pins being used.

 

#include <Wire.h>
#include "RTClib.h"
#include <LiquidCrystal.h>
#include <Password.h>
#include <Keypad.h>
#include <Adafruit_Fingerprint.h>
#if ARDUINO >= 100
 #include <SoftwareSerial.h>
#else
 #include <NewSoftSerial.h>
#endif


RTC_DS1307 RTC;


LiquidCrystal lcd(15, 14, 13, 12, 11, 10);


int getFingerprintIDez();
const int lockPin = 18;
const int lcdRed = 15;
const int lcdGreen = 16;
const int lcdBlue = 17;
const int buttonPin = 2;
const int [p


int buttonState = 0;


// pin #1 is IN from sensor (GREEN wire)
// pin #2 is OUT from arduino  (WHITE wire)
#if ARDUINO >= 100
SoftwareSerial mySerial(1, 2);
#else
NewSoftSerial mySerial(1, 2);
#endif


Adafruit_Fingerprint finger = Adafruit_Fingerprint(&mySerial);


Password password = Password( "1234" );


const byte ROWS = 4; // Four rows
const byte COLS = 3; //  columns
// Define the Keymap
char keys[ROWS][COLS] = {
  {'1','2','3'},
  {'4','5','6'},
  {'7','8','9'},
  {'*','0','#'}
};


byte rowPins[ROWS] = { 9,8,7,6 };// Connect keypad ROW0, ROW1, ROW2 and ROW3 to these Arduino pins.
byte colPins[COLS] = { 5,4,3 };// Connect keypad COL0, COL1 and COL2 to these Arduino pins.


// Create the Keypad
Keypad keypad = Keypad( makeKeymap(keys), rowPins, colPins, ROWS, COLS );


void setup()  
{
  pinMode(lockPin, OUTPUT);
  pinMode(lcdRed, OUTPUT);
  pinMode(lcdGreen, OUTPUT);
  pinMode(lcdBlue, OUTPUT);
  pinMode(buttonPin, INPUT);  
  
  lcd.begin(16, 2);
  Serial.begin(9600);
  keypad.addEventListener(keypadEvent); //add an event listener for this keypad
  Serial.println("fingertest");


  // set the data rate for the sensor serial port
  finger.begin(57600);
  
  if (finger.verifyPassword()) {
    Serial.println("Found fingerprint sensor!");
  } else {
    Serial.println("Did not find fingerprint sensor :(");
    while (1);
  }
  DateTime now = RTC.now();
  Serial.println("Waiting for valid finger...");
  lcd.noCursor();
  lcd.clear();
  lcd.print("HENRYS WORK ROOM");
  lcd.setCursor(5, 1);
  lcd.print(now.hour(), DEC);
  lcd.setCursor(7, 1);
  lcd.print(":");
  lcd.print(now.minute(), DEC);
  digitalWrite(lcdRed, LOW);
  digitalWrite(lcdGreen, LOW);
  digitalWrite(lcdBlue, HIGH);
  digitalWrite(lockPin, HIGH);
}


void loop() // run over and over again
{
  getFingerprintIDez();
  keypad.getKey();
  buttonState = digitalRead(buttonPin);
}
//take care of some special events
void keypadEvent(KeypadEvent eKey){
  switch (keypad.getState()){
    case PRESSED:
  Serial.print("Pressed: ");
  Serial.println(eKey);
  switch (eKey){
   case '*': checkPassword(); break;
   case '#': password.reset(); break;
   default: password.append(eKey);
     }
  }
} 


void checkPassword(){
  if (password.evaluate()){
    Serial.println("Success");
    //Add code to run if it works
    DateTime now = RTC.now();
    lcd.clear();
    lcd.print("ACCESS GRANTED");
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdBlue, LOW);
    digitalWrite(lcdGreen, HIGH);
    digitalWrite(lockPin, LOW);
    delay(10000);
    lcd.clear();
    digitalWrite(lockPin, HIGH);
    lcd.print("HENRYS WORK ROOM");
    lcd.setCursor(5, 1);
    lcd.print(now.hour(), DEC);
    lcd.setCursor(7, 1);
    lcd.print(":");
    lcd.print(now.minute(), DEC);
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdBlue, HIGH);
    
  }else{
    DateTime now = RTC.now();
    Serial.println("Wrong");
    lcd.clear();
    lcd.print("ACCESS DENIED");
    digitalWrite(lcdBlue, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdRed, HIGH);
    digitalWrite(lockPin, HIGH);
    delay(10000);
    lcd.clear();
    lcd.print("HENRYS WORK ROOM");
    lcd.setCursor(5, 1);
    lcd.print(now.hour(), DEC);
    lcd.setCursor(7, 1);
    lcd.print(":");
    lcd.print(now.minute(), DEC);
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdBlue, HIGH);
    digitalWrite(lockPin, HIGH);
  }
}


uint8_t getFingerprintID() {
  uint8_t p = finger.getImage();
  switch (p) {
    case FINGERPRINT_OK:
      Serial.println("Image taken");
      break;
    case FINGERPRINT_NOFINGER:
      Serial.println("No finger detected");
      return p;
    case FINGERPRINT_PACKETRECIEVEERR:
      Serial.println("Communication error");
      return p;
    case FINGERPRINT_IMAGEFAIL:
      Serial.println("Imaging error");
      return p;
    default:
      Serial.println("Unknown error");
      return p;
  }


  // OK success!


  p = finger.image2Tz();
  switch (p) {
    case FINGERPRINT_OK:
      Serial.println("Image converted");
      break;
    case FINGERPRINT_IMAGEMESS:
      Serial.println("Image too messy");
      return p;
    case FINGERPRINT_PACKETRECIEVEERR:
      Serial.println("Communication error");
      return p;
    case FINGERPRINT_FEATUREFAIL:
      Serial.println("Could not find fingerprint features");
      return p;
    case FINGERPRINT_INVALIDIMAGE:
      Serial.println("Could not find fingerprint features");
      return p;
    default:
      Serial.println("Unknown error");
      return p;
  }
  
  // OK converted!
  p = finger.fingerFastSearch();
  if (p == FINGERPRINT_OK) {
    Serial.println("Found a print match!");
  } else if (p == FINGERPRINT_PACKETRECIEVEERR) {
    Serial.println("Communication error");
    return p;
  } else if (p == FINGERPRINT_NOTFOUND) {
    Serial.println("Did not find a match");
    
    DateTime now = RTC.now();
    Serial.println("Wrong");
    lcd.clear();
    lcd.print("ACCESS DENIED");
    digitalWrite(lcdBlue, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdRed, HIGH);
    digitalWrite(lockPin, HIGH);
    delay(10000);
    lcd.clear();
    lcd.print("HENRYS WORK ROOM");
    lcd.setCursor(5, 1);
    lcd.print(now.hour(), DEC);
    lcd.setCursor(7, 1);
    lcd.print(":");
    lcd.print(now.minute(), DEC);
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdBlue, HIGH);
    digitalWrite(lockPin, HIGH);
    return p;
  } else {
    Serial.println("Unknown error");
    
    DateTime now = RTC.now();
    Serial.println("Wrong");
    lcd.clear();
    lcd.print("Unknown error");
    digitalWrite(lcdBlue, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdRed, HIGH);
    digitalWrite(lockPin, HIGH);
    delay(10000);
    lcd.clear();
    lcd.print("HENRYS WORK ROOM");
    lcd.setCursor(5, 1);
    lcd.print(now.hour(), DEC);
    lcd.setCursor(7, 1);
    lcd.print(":");
    lcd.print(now.minute(), DEC);
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdBlue, HIGH);
    digitalWrite(lockPin, HIGH);
    return p;
  }   
  
  // found a match!
  Serial.print("Found ID #"); Serial.print(finger.fingerID); 
  Serial.print(" with confidence of "); Serial.println(finger.confidence);
}


// returns -1 if failed, otherwise returns ID #
int getFingerprintIDez() {
  uint8_t p = finger.getImage();
  if (p != FINGERPRINT_OK)  return -1;


  p = finger.image2Tz();
  if (p != FINGERPRINT_OK)  return -1;


  p = finger.fingerFastSearch();
  if (p != FINGERPRINT_OK)  return -1;
  
  // found a match!
    DateTime now = RTC.now();
    
    lcd.clear();
    lcd.print("ACCESS GRANTED");
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdBlue, LOW);
    digitalWrite(lcdGreen, HIGH);
    digitalWrite(lockPin, LOW);
    delay(10000);
    lcd.clear();
    digitalWrite(lockPin, LOW);
    lcd.print("HENRYS WORK ROOM");
    lcd.setCursor(5, 1);
    lcd.print(now.hour(), DEC);
    lcd.setCursor(7, 1);
    lcd.print(":");
    lcd.print(now.minute(), DEC);
    digitalWrite(lcdRed, LOW);
    digitalWrite(lcdGreen, LOW);
    digitalWrite(lcdBlue, HIGH);
    digitalWrite(lockPin, HIGH);
    
  Serial.print("Found ID #"); Serial.print(finger.fingerID); 
  Serial.print(" with confidence of "); Serial.println(finger.confidence);
  return finger.fingerID; 
}

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    PLEASE DISREGARD

    const int [p


    that can be deleted

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    same with pinMode(buttonPin, INPUT); ,  const int buttonPin = 2;   and any thing else regarding a button

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    same with pinMode(buttonPin, INPUT); ,  const int buttonPin = 2;   and any thing else regarding a button