Arduino
  • Products
  • More
Arduino
Arduino Forum Basic Circuitry Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 561 views
  • Users 0 members are here
  • help
  • simple_circuit
  • resistor
  • arduino
Related

Basic Circuitry Questions

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I recently began making circuits with Arduino Uno and I had a couple basic questions about the circuits I have made.

 

1) The first is that for all of the circuits I have put together, I am told to run a wire from the 5V power output to the side column of the breadboard. However, even when I unplug this wire the circuit still runs and seems as though the power doesn't have to be supplied. Is there already being power supplied through the output pins I have set up?

 

2) I understand that these circuits begin with the pin output and end with the ground. So I would think that if the led's needed a resistor, it would be before the led (on the side closer to the pin). This seems to be true for about half of the circuit diagrams I have seen, in several of the circuit diagrams the resistor is after the led. I attached pictures showing two diagrams showing each of these scenarios. Why is it different in these two cases? Why would the resistor be after the led?

 

Thanks a lot

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • billpenner
    0 billpenner over 12 years ago

    Hi Bill Here.

    With out the complete circuit I cannot be sure but;

    In the first circuit.. if you are using a USB to the computer, the USB probably supplies the power for the circuit.

    In the second circuit, Since both the LED and the resister are in series,  all the current goes through both.

    So it makes no difference what is the order the components are connected.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 12 years ago

    Hi Bill Here.

    With out the complete circuit I cannot be sure but;

    In the first circuit.. if you are using a USB to the computer, the USB probably supplies the power for the circuit.

    In the second circuit, Since both the LED and the resister are in series,  all the current goes through both.

    So it makes no difference what is the order the components are connected.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer