Arduino
  • Products
  • More
Arduino
Arduino Forum Basic Circuitry Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 561 views
  • Users 0 members are here
  • help
  • simple_circuit
  • resistor
  • arduino
Related

Basic Circuitry Questions

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I recently began making circuits with Arduino Uno and I had a couple basic questions about the circuits I have made.

 

1) The first is that for all of the circuits I have put together, I am told to run a wire from the 5V power output to the side column of the breadboard. However, even when I unplug this wire the circuit still runs and seems as though the power doesn't have to be supplied. Is there already being power supplied through the output pins I have set up?

 

2) I understand that these circuits begin with the pin output and end with the ground. So I would think that if the led's needed a resistor, it would be before the led (on the side closer to the pin). This seems to be true for about half of the circuit diagrams I have seen, in several of the circuit diagrams the resistor is after the led. I attached pictures showing two diagrams showing each of these scenarios. Why is it different in these two cases? Why would the resistor be after the led?

 

Thanks a lot

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Rick,

    You have two good answers to your question but I thought that I might add that if you are looking for a book that has a good section on beginning electronics and circuit design you might want to check out "Practical Electronics for Inventors"  by Paul Scherz and Simon Monk. There are three editions out. You can probably check out ebay if you want to save a little money. I would recommend the third edition as it has sections on microprocessors and interfacing with them. The earlier edition had a reputation of a lot of errata but the 3rd seems much improved. Good luck on you adventure in electronics.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago

    Hi Rick,

    You have two good answers to your question but I thought that I might add that if you are looking for a book that has a good section on beginning electronics and circuit design you might want to check out "Practical Electronics for Inventors"  by Paul Scherz and Simon Monk. There are three editions out. You can probably check out ebay if you want to save a little money. I would recommend the third edition as it has sections on microprocessors and interfacing with them. The earlier edition had a reputation of a lot of errata but the 3rd seems much improved. Good luck on you adventure in electronics.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer