Arduino
  • Products
  • More
Arduino
Arduino Forum Basic Circuitry Questions
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 559 views
  • Users 0 members are here
  • help
  • simple_circuit
  • resistor
  • arduino
Related

Basic Circuitry Questions

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I recently began making circuits with Arduino Uno and I had a couple basic questions about the circuits I have made.

 

1) The first is that for all of the circuits I have put together, I am told to run a wire from the 5V power output to the side column of the breadboard. However, even when I unplug this wire the circuit still runs and seems as though the power doesn't have to be supplied. Is there already being power supplied through the output pins I have set up?

 

2) I understand that these circuits begin with the pin output and end with the ground. So I would think that if the led's needed a resistor, it would be before the led (on the side closer to the pin). This seems to be true for about half of the circuit diagrams I have seen, in several of the circuit diagrams the resistor is after the led. I attached pictures showing two diagrams showing each of these scenarios. Why is it different in these two cases? Why would the resistor be after the led?

 

Thanks a lot

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I appreciate the responses, thanks a lot. I guess I was just overthinking it. I'll definitely take a look at that book though

     

    RIck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I appreciate the responses, thanks a lot. I guess I was just overthinking it. I'll definitely take a look at that book though

     

    RIck