Arduino Forum Hola, tengo un proyecto con un giroscopio ayuda por favor!
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 392 subscribers
  • Views 307 views
  • Users 0 members are here
  • novato
  • giroscopio
  • arduino
Related

Hola, tengo un proyecto con un giroscopio ayuda por favor!

Former Member
Former Member over 11 years ago

Mi proyecto es con un arduino uno con el cual planeo hacer un head mounted display, me pongo el giroscopio en la cabeza y con la rotacion de x e y hago que dos servo motores giren al mismo tiempo con los valores obtenidos por el giroscopio.

Por ahora voy a usar un joystick para hacer que rote estilo call of duty.

 

Ademas quiero saber cuales son las herramientas y materiales que necesitare para hacer que el giroscopio funcione.

 

Soy nuevo en element14 por favor ayuda.

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hola Mael,

     

    Bienvenido al communidad de E-14. Aunque  puedo endender su pregunta no tengo experiencia sufficiente a ayudarle. Voy a traducir su mensaje en esperanza que los que hablan ingles tendran consejos. Buena suerte con su proyecto.

     

    John

     

    Translation of Mael's Question: My project is with an Arduino Uno with which I plan to make a head mounted display, I will place the gyroscope in the head and with two servo motors that turn at the same time I will make the x - y rotation using values that I obtain from the gyroscope.  For now I am going to use a joystick in the manner of Call of Duty. I would like to know what type of materials and tools I will need to make the gyroscope function. I am new to Element 14 , please help me.

     

    End of translation by John. Apologies if it isn't exact as my Spanish isn't much better than my electronics ability.

     

    Perhaps someone has some links to help Mael with his project.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hola Mael,

     

    Bienvenido al communidad de E-14. Aunque  puedo endender su pregunta no tengo experiencia sufficiente a ayudarle. Voy a traducir su mensaje en esperanza que los que hablan ingles tendran consejos. Buena suerte con su proyecto.

     

    John

     

    Translation of Mael's Question: My project is with an Arduino Uno with which I plan to make a head mounted display, I will place the gyroscope in the head and with two servo motors that turn at the same time I will make the x - y rotation using values that I obtain from the gyroscope.  For now I am going to use a joystick in the manner of Call of Duty. I would like to know what type of materials and tools I will need to make the gyroscope function. I am new to Element 14 , please help me.

     

    End of translation by John. Apologies if it isn't exact as my Spanish isn't much better than my electronics ability.

     

    Perhaps someone has some links to help Mael with his project.

     

    Thanks