Arduino
  • Products
  • More
Arduino
Arduino Forum using XBees with Arduino, a question...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 273 views
  • Users 0 members are here
Related

using XBees with Arduino, a question...

kjhart0133
kjhart0133 over 12 years ago

I'm using an Arduino Uno and two XBee S2 modules to set up a wireless system to remotely control heating and lighting in a distant building (a workshop.)  After many hours of learning how to run the two wireless modules in API mode, I'm now at the point where I can construct and read frames sent wirelessly between the two modules.  I do still have a couple of questions on the XBee operation, but I'm not sure if this is the right forum to pose those questions.  I looked in the "Wireless" discussion area, but that didn't seem like the right place.  Can someone steer me to an appropriate discussion group on XBees; or maybe this is as good a place as any to ask questions.

 

My first question would be:

 

I'm instructing the coordinator XBee to send an IS command (Force Sample) to the router XBee using Frame Type 0x17, a Remote AT Command Request.  I'm expecting possibly two responses from the remote: 1) Frame Type 0x97, a Remote Command Response; and 2) Frame Type 0x92, an I/O Data Sample Rx Response.  Is it true that I can expect both Frames from the remote, and if so, which Frame is sent to the coordinator XBee first?

 

I will have more questions down the road, but I don't want to clog up the forum if this is not the place for this discussion.

 

Thanks,

 

Kevin H.

  • Sign in to reply
  • Cancel
Parents
  • kjhart0133
    0 kjhart0133 over 12 years ago

    Nevermind! I figured it out.

     

    It turns out when you send an IS command using Remote AT Command Req., (Frame Type 0x17), the remote XBee responds with a single Remote Cmd Response (Frame Type 0x97) that contains data for all the programmed I/O pins, both digital and analog pins.

     

    This question is answered.

     

    Thanks,

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • kjhart0133
    0 kjhart0133 over 12 years ago

    Nevermind! I figured it out.

     

    It turns out when you send an IS command using Remote AT Command Req., (Frame Type 0x17), the remote XBee responds with a single Remote Cmd Response (Frame Type 0x97) that contains data for all the programmed I/O pins, both digital and analog pins.

     

    This question is answered.

     

    Thanks,

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer