Arduino
  • Products
  • More
Arduino
Arduino Forum help arduino code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 574 views
  • Users 0 members are here
  • arduino
Related

help arduino code

nmmbeginer
nmmbeginer over 12 years ago

i found this http://wordpress.codewrite.co.uk/pic/2014/01/21/cap-meter-with-arduino-uno/ project on line when i open the Seiral moniter this is what i get     ÁŒüš› ü .#ÿ Á þh Rÿ .#ÿÛOËüè  ÿ°ÕF`££ü¸OKü¸OKü

so if some one can tell me how to fix this please let me know.

 

hear is the code i used

 

 

const int OUT_PIN = A2;

const int IN_PIN = A0;

 

 

//Capacitance between IN_PIN and Ground

//Stray capacitance is always present. Extra capacitance can be added to

//allow higher capacitance to be measured.

const float IN_STRAY_CAP_TO_GND = 24.48; //initially this was 30.00

const float IN_EXTRA_CAP_TO_GND = 0.0;

const float IN_CAP_TO_GND  = IN_STRAY_CAP_TO_GND + IN_EXTRA_CAP_TO_GND;

const int MAX_ADC_VALUE = 1023;

 

 

void setup()

{

  pinMode(OUT_PIN, OUTPUT);

  //digitalWrite(OUT_PIN, LOW);  //This is the default state for outputs

  pinMode(IN_PIN, OUTPUT);

  //digitalWrite(IN_PIN, LOW);

 

 

  Serial.begin(115200);

}

 

 

void loop()

{

  //Capacitor under test between OUT_PIN and IN_PIN

  //Rising high edge on OUT_PIN

  pinMode(IN_PIN, INPUT);

  digitalWrite(OUT_PIN, HIGH);

  int val = analogRead(IN_PIN);

 

 

  //Clear everything for next measurement

  digitalWrite(OUT_PIN, LOW);

  pinMode(IN_PIN, OUTPUT);

 

 

  //Calculate and print result

 

 

  float capacitance = (float)val * IN_CAP_TO_GND / (float)(MAX_ADC_VALUE - val);

 

 

  Serial.print(F("Capacitance Value = "));

  Serial.print(capacitance, 3);

  Serial.print(F(" pF ("));

  Serial.print(val);

  Serial.println(F(") "));

 

 

  while (millis() % 500 != 0)

    ;   

}

  • Sign in to reply
  • Cancel
Parents
  • klong84
    0 klong84 over 12 years ago

    Hi, check baud-rate. They are not equal B/W serial monitor and code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • nmmbeginer
    0 nmmbeginer over 12 years ago in reply to klong84

    thanks works great now

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nmmbeginer
    0 nmmbeginer over 12 years ago in reply to klong84

    thanks works great now