Arduino Forum Arduino relays for lighting
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
  • State Suggested Answer
  • Replies 17 replies
  • Answers 3 answers
  • Subscribers 405 subscribers
  • Views 2513 views
  • Users 0 members are here
  • lighting
  • relays
  • arduino
Related

Arduino relays for lighting

Former Member
Former Member over 11 years ago

All,

 

I'm building a new house, and I decided that I want microcontrollers to control my lighting. Now I have dimmers covered, with a 0-+10V system, but surprisingly I'm struggling a bit with the lights that should just be on or off. I figured it should be doable with a relatively cheap array of relays connected to an Arduino. I'm not going to get my hands dirty, my electrician is (which is, I should say, a good idea). He insists on the following standard for the relays:

  • CE certification.
  • at least 240 VAC
  • at least 10A
  • DIN Rail mountable

 

I'm guessing I could satisfy the last requirement with a PCB in something like this: http://cpc.farnell.com/pulse/acc-case-m/flightcase-universal-medium/dp/DP31699

I have not yet found a product, that matches all of the top three though: I found something in various shops that has 250 VAC @ 10A, but no visible CE mark, and I found one on hobbyking http://hobbyking.com/hobbyking/store/__26921__Arduino_6_Channel_Relay_Module.html that had a CE mark, but could only do 240VAC @ 7A. I'd like something like that, with 6-8 channels would be nice.

 

It would be nice if the electrician could order all the products from Farnell, since they have a Norwegian office and I have used them for some other projects. Any pointers?

 

Message was edited by: Matt Collinge. Updated CPC link.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +2
    Your electrician is right in terms of good practice and it may well be that local laws require the parts to comply with his suggestions. I expect you would like your house to last at least 25 years before…
  • beacon_dave
    beacon_dave over 9 years ago in reply to michaelkellett +2 suggested
    Michael Kellett wrote: ...Arduino isn't the right kind of thing for this - I think you should go for industrial standard parts and practice which would suggest 24V DC relay coils... There are these Arduino…
  • shabaz
    shabaz over 9 years ago in reply to mcb1 +2
    There are even more possibilities, like activation without taking the device out the package : ) (I've no idea if Peter's device does that, but technically it is feasible). NXP has a part which can be…
Parents
  • dougw
    0 dougw over 9 years ago

    Farnell carries lots of optically isolated solid state relays that meet your specs:

    here are a few of them:

    861SSR210-DC-1 SCHNEIDER ELECTRIC/MAGNECRAFT, Solid State Relay, SPST-NO, 10 A, DIN Rail, Screw, 24 VAC, 280 VAC, Newark…

    RA2410-D06T CARLO GAVAZZI, Solid State Relay, SPST-NO, 10 A, DIN Rail, Quick Connect, 24 VAC, 280 VAC, Newark element14 …

    SSR210DIN-DC22 SCHNEIDER ELECTRIC/MAGNECRAFT, Solid State Relay, SPST-NO, 10 A, DIN Rail, Screw, 24 VAC, 280 VAC, Newark…

    CKRD2410 CRYDOM, Solid State Relay, SPST-NO, 10 A, DIN Rail, Cage Clamp, 24 Vrms, 280 Vrms, Newark element14 Canada

    861SSR210-AC-1 SCHNEIDER ELECTRIC/MAGNECRAFT, Solid State Relay, SPST-NO, 10 A, DIN Rail, Screw, 24 VAC, 280 VAC, Newark…

    CKRD2420 CRYDOM, Solid State Relay, SPST-NO, 20 A, DIN Rail, Cage Clamp, 24 Vrms, 280 Vrms, Newark element14 Canada

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 9 years ago

    Farnell carries lots of optically isolated solid state relays that meet your specs:

    here are a few of them:

    861SSR210-DC-1 SCHNEIDER ELECTRIC/MAGNECRAFT, Solid State Relay, SPST-NO, 10 A, DIN Rail, Screw, 24 VAC, 280 VAC, Newark…

    RA2410-D06T CARLO GAVAZZI, Solid State Relay, SPST-NO, 10 A, DIN Rail, Quick Connect, 24 VAC, 280 VAC, Newark element14 …

    SSR210DIN-DC22 SCHNEIDER ELECTRIC/MAGNECRAFT, Solid State Relay, SPST-NO, 10 A, DIN Rail, Screw, 24 VAC, 280 VAC, Newark…

    CKRD2410 CRYDOM, Solid State Relay, SPST-NO, 10 A, DIN Rail, Cage Clamp, 24 Vrms, 280 Vrms, Newark element14 Canada

    861SSR210-AC-1 SCHNEIDER ELECTRIC/MAGNECRAFT, Solid State Relay, SPST-NO, 10 A, DIN Rail, Screw, 24 VAC, 280 VAC, Newark…

    CKRD2420 CRYDOM, Solid State Relay, SPST-NO, 20 A, DIN Rail, Cage Clamp, 24 Vrms, 280 Vrms, Newark element14 Canada

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer