Arduino
  • Products
  • More
Arduino
Arduino Forum Ethernet Shield error
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Subscribers 417 subscribers
  • Views 3419 views
  • Users 0 members are here
  • arduino
Related

Ethernet Shield error

e14 Contributor
e14 Contributor over 12 years ago

I am using below Open source Code to test my Ethernet sheild connected to Uno . Seems Everything is fine  but when I try to compile or upload its comming up with error ; 'Ethernet has not been declared' and There are few other error probally causing because of the Main error ;

rbbb_server:11: error: 'Ethernet' has not been declared

rbbb_server:12: error: 'BufferFiller' does not name a type

rbbb_server.ino: In function 'void setup()':

rbbb_server:15: error: 'ether' was not declared in this scope

rbbb_server:15: error: 'Ethernet' has not been declared

rbbb_server:17: error: 'ether' was not declared in this scope

rbbb_server.ino: In function 'word homePage()':

rbbb_server:25: error: 'bfill' was not declared in this scope

rbbb_server:25: error: 'ether' was not declared in this scope

rbbb_server.ino: In function 'void loop()':

rbbb_server:39: error: 'ether' was not declared in this scope.

 

if someone can help me fix this issues it will be grateful Thank you

 

// This is a demo of the RBBB running as webserver with the Ether Card

// 2010-05-28 <jc@wippler.nl> http://opensource.org/licenses/mit-license.php

 

 

 

//#include <Ethernet.h>

#include <EtherCard.h>

 

 

// ethernet interface mac address, must be unique on the LAN

static byte mymac[] = { 0x74,0x69,0x69,0x2D,0x30,0x31 };

static byte myip[] = { 192,168,1,203 };

 

 

byte Ethernet::buffer[500];

BufferFiller bfill;

 

 

void setup () {

  if (ether.begin(sizeof Ethernet::buffer, mymac) == 0)

    Serial.println( "Failed to access Ethernet controller");

  ether.staticSetup(myip);

}

 

 

static word homePage() {

  long t = millis() / 1000;

  word h = t / 3600;

  byte m = (t / 60) % 60;

  byte s = t % 60;

  bfill = ether.tcpOffset();

  bfill.emit_p(PSTR(

    "HTTP/1.0 200 OK\r\n"

    "Content-Type: text/html\r\n"

    "Pragma: no-cache\r\n"

    "\r\n"

    "<meta http-equiv='refresh' content='1'/>"

    "<title>RBBB server</title>"

    "<h1>$D$D:$D$D:$D$D</h1>"),

      h/10, h%10, m/10, m%10, s/10, s%10);

  return bfill.position();

}

 

 

void loop () {

  word len = ether.packetReceive();

  word pos = ether.packetLoop(len);

 

  if (pos)  // check if valid tcp data is received

    ether.httpServerReply(homePage()); // send web page data

}

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Have you verified you have the correct library installed in the library folder for the IDE

     

    What Shield are you using, I would assume it would be a WizNet 5100 based shield but please confirm

     

    Based on the fact your getting the errors including the include itself, this would imply the compiler can not find the library

     

    WizNet is I believe fully supported by the default IDE libraries, the reason I ask it that you comment out ethernet.h and replaced with ethercard.h, why was this and does the other one work ?

     

    ethercard may be for the ENC chip Ethernet controller and would need you to actually download the library if your using that device of course.

     

    regards

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hi Sorry I meant I am using W5100? wiznet Ethernet sheild and rbbb server example doesnt work Its uploads but doesnt work ?

     

     

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    Unfortunately the ENC and the WIZ boards are very different in their design, yes they both provide internet functionality but the code used to make them work is not compatible at the sketch level, you have to adjust the programming to work on the other

     

    the fortunate thing is that it is easier to go from a ENC to Wiz rather than the other way around

     

    If i get a chance over the weekend I will look at your code to see if I can help you fix it

     

    till then, have fun, and good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    ?Thank you sir

     

     

    Regards

     

    Ankit Patel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    ?Thank you sir

     

     

    Regards

     

    Ankit Patel