Arduino
  • Products
  • More
Arduino
Arduino Forum Ethernet Shield error
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Subscribers 417 subscribers
  • Views 3419 views
  • Users 0 members are here
  • arduino
Related

Ethernet Shield error

e14 Contributor
e14 Contributor over 12 years ago

I am using below Open source Code to test my Ethernet sheild connected to Uno . Seems Everything is fine  but when I try to compile or upload its comming up with error ; 'Ethernet has not been declared' and There are few other error probally causing because of the Main error ;

rbbb_server:11: error: 'Ethernet' has not been declared

rbbb_server:12: error: 'BufferFiller' does not name a type

rbbb_server.ino: In function 'void setup()':

rbbb_server:15: error: 'ether' was not declared in this scope

rbbb_server:15: error: 'Ethernet' has not been declared

rbbb_server:17: error: 'ether' was not declared in this scope

rbbb_server.ino: In function 'word homePage()':

rbbb_server:25: error: 'bfill' was not declared in this scope

rbbb_server:25: error: 'ether' was not declared in this scope

rbbb_server.ino: In function 'void loop()':

rbbb_server:39: error: 'ether' was not declared in this scope.

 

if someone can help me fix this issues it will be grateful Thank you

 

// This is a demo of the RBBB running as webserver with the Ether Card

// 2010-05-28 <jc@wippler.nl> http://opensource.org/licenses/mit-license.php

 

 

 

//#include <Ethernet.h>

#include <EtherCard.h>

 

 

// ethernet interface mac address, must be unique on the LAN

static byte mymac[] = { 0x74,0x69,0x69,0x2D,0x30,0x31 };

static byte myip[] = { 192,168,1,203 };

 

 

byte Ethernet::buffer[500];

BufferFiller bfill;

 

 

void setup () {

  if (ether.begin(sizeof Ethernet::buffer, mymac) == 0)

    Serial.println( "Failed to access Ethernet controller");

  ether.staticSetup(myip);

}

 

 

static word homePage() {

  long t = millis() / 1000;

  word h = t / 3600;

  byte m = (t / 60) % 60;

  byte s = t % 60;

  bfill = ether.tcpOffset();

  bfill.emit_p(PSTR(

    "HTTP/1.0 200 OK\r\n"

    "Content-Type: text/html\r\n"

    "Pragma: no-cache\r\n"

    "\r\n"

    "<meta http-equiv='refresh' content='1'/>"

    "<title>RBBB server</title>"

    "<h1>$D$D:$D$D:$D$D</h1>"),

      h/10, h%10, m/10, m%10, s/10, s%10);

  return bfill.position();

}

 

 

void loop () {

  word len = ether.packetReceive();

  word pos = ether.packetLoop(len);

 

  if (pos)  // check if valid tcp data is received

    ether.httpServerReply(homePage()); // send web page data

}

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Im Back, Had a look at your code, updated it to make it work, here is a video of the results

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    The ENC28J60 does not directly support TCP/IP and requires a far larger library in order to implement it, the WIZ chip has firmware TCP/IP stack built in and supports several concurrent sessions

     

    the Older ENC library was also incompatible with the default Arduino Library created to support the Wiznet chip

     

    I hear there is now a later version that has been re-worked to be fully compatible so if you want maximum flexibility then you should adopt this new ENC library

     

    You can find it here: https://github.com/ntruchsess/arduino_uip


    here is the adapted code based on your posted code to work on the WizNet board


    #include <SPI.h>
    #include <Wire.h>
    #include <stdio.h>
    #include <Ethernet.h>
    //#include <EtherCard.h>
    
    // ethercard interface mac address, must be unique on the LAN
    //static byte mymac[] = { 0x74,0x69,0x69,0x2D,0x30,0x31 };
    //static byte myip[] = { 192,168,1,203 };
    // byte Ethernet::buffer[500];
            
    //ethernet
    byte mac[] = { 0x90, 0xA2, 0xDA, 0x00, 0x4E, 0x10 };  // MAC address 84.85.88.16.0.36
    byte ip[]  = { 192, 168, 1, 203 };                     // ip-address, please change to fit your network
    byte mydns[] = { 192, 168, 1, 1 };          
    byte gateway[] = { 192, 168, 1, 1 };           
    byte subnet[] = { 255,255,255,0 };
    EthernetServer server(80);
    static char output[300] = "";
    #define BUFLEN 255
    
    
    //BufferFiller bfill;
    
    
    void setup () {
    //ethercard
    // if (ether.begin(sizeof Ethernet::buffer, mymac) == 0)
    //   Serial.println( "Failed to access Ethernet controller");
    //ether.staticSetup(myip);
      Serial.begin(9600);
      //ethernet
      Ethernet.begin(mac, ip);
      server.begin();
      Serial.print("server is at ");
      Serial.println(Ethernet.localIP());
    }
    char headerHTML[] = "HTTP/1.1 200 OK\r\n"
              "Content-Type: text/html\r\n"
              "Connection: close\r\n"
              "Refresh: 5\r\n"
              "\r\n"
              "<!DOCTYPE HTML>"
              "<Title>RBBS Server</Title>"
              "<html>";
            
    char footerHTML[] = "</html>" ;
    
    char * TimeElapsed() { // Was Home Page
      long t = millis() / 1000;
      word h = t / 3600;
      byte m = (t / 60) % 60;
      byte s = t % 60;
      sprintf(output, "<h1>%d%d:%d%d:%d%d</h1>" , h/10, h%10, m/10, m%10, s/10, s%10);
      return output;
    }
    
    void sendAnalogToNetwork(EthernetClient myClient)
    {
        // output the value of each analog input pin for good measure
        for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
          int sensorReading = analogRead(analogChannel);
          myClient.print("analog input ");
          myClient.print(analogChannel);
          myClient.print(" is ");
          myClient.print(sensorReading);
          myClient.println("<br />");     
        }
    }
    
    void loop ()
    {
    // listen for incoming clients
      EthernetClient client = server.available();
      if (client) {
        Serial.println("new client");
        // an http request ends with a blank line
        boolean currentLineIsBlank = true;
        while (client.connected()) {
          if (client.available()) {
            char c = client.read();
            Serial.write(c);
            // if you've gotten to the end of the line (received a newline
            // character) and the line is blank, the http request has ended,
            // so you can send a reply
            if (c == '\n' && currentLineIsBlank) {
              // send a standard http response header
              client.print(headerHTML);
              // now send the stuff we want
              client.print(TimeElapsed()); // your old code here
              // do some more stuff
              sendAnalogToNetwork(client);
               // were done sending so now send the footer to close the page
              client.println(footerHTML);
              break;
            }
            if (c == '\n') {
              // you're starting a new line
              currentLineIsBlank = true;
            }
            else if (c != '\r') {
              // you've gotten a character on the current line
              currentLineIsBlank = false;
            }
          }
        }
        // give the web browser time to receive the data
        delay(1);
        // close the connection:
        client.stop();
        Serial.println("client disconnected");
      }
    }

     

    As you can see I have also provided a bit of re-formatting of the code to use more functions and variables for the constant strings, it could be better but it does demonstrate how the code needs to work on the Wiznet and also a few tips on program design

     

    I hope it meets your needs and gets you going int the right direction

     

    If this is the right Answer for you then please click "Correct Answer", thanks

    Attachments:
    RBBS_Server_Update.ino.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Im Back, Had a look at your code, updated it to make it work, here is a video of the results

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    The ENC28J60 does not directly support TCP/IP and requires a far larger library in order to implement it, the WIZ chip has firmware TCP/IP stack built in and supports several concurrent sessions

     

    the Older ENC library was also incompatible with the default Arduino Library created to support the Wiznet chip

     

    I hear there is now a later version that has been re-worked to be fully compatible so if you want maximum flexibility then you should adopt this new ENC library

     

    You can find it here: https://github.com/ntruchsess/arduino_uip


    here is the adapted code based on your posted code to work on the WizNet board


    #include <SPI.h>
    #include <Wire.h>
    #include <stdio.h>
    #include <Ethernet.h>
    //#include <EtherCard.h>
    
    // ethercard interface mac address, must be unique on the LAN
    //static byte mymac[] = { 0x74,0x69,0x69,0x2D,0x30,0x31 };
    //static byte myip[] = { 192,168,1,203 };
    // byte Ethernet::buffer[500];
            
    //ethernet
    byte mac[] = { 0x90, 0xA2, 0xDA, 0x00, 0x4E, 0x10 };  // MAC address 84.85.88.16.0.36
    byte ip[]  = { 192, 168, 1, 203 };                     // ip-address, please change to fit your network
    byte mydns[] = { 192, 168, 1, 1 };          
    byte gateway[] = { 192, 168, 1, 1 };           
    byte subnet[] = { 255,255,255,0 };
    EthernetServer server(80);
    static char output[300] = "";
    #define BUFLEN 255
    
    
    //BufferFiller bfill;
    
    
    void setup () {
    //ethercard
    // if (ether.begin(sizeof Ethernet::buffer, mymac) == 0)
    //   Serial.println( "Failed to access Ethernet controller");
    //ether.staticSetup(myip);
      Serial.begin(9600);
      //ethernet
      Ethernet.begin(mac, ip);
      server.begin();
      Serial.print("server is at ");
      Serial.println(Ethernet.localIP());
    }
    char headerHTML[] = "HTTP/1.1 200 OK\r\n"
              "Content-Type: text/html\r\n"
              "Connection: close\r\n"
              "Refresh: 5\r\n"
              "\r\n"
              "<!DOCTYPE HTML>"
              "<Title>RBBS Server</Title>"
              "<html>";
            
    char footerHTML[] = "</html>" ;
    
    char * TimeElapsed() { // Was Home Page
      long t = millis() / 1000;
      word h = t / 3600;
      byte m = (t / 60) % 60;
      byte s = t % 60;
      sprintf(output, "<h1>%d%d:%d%d:%d%d</h1>" , h/10, h%10, m/10, m%10, s/10, s%10);
      return output;
    }
    
    void sendAnalogToNetwork(EthernetClient myClient)
    {
        // output the value of each analog input pin for good measure
        for (int analogChannel = 0; analogChannel < 6; analogChannel++) {
          int sensorReading = analogRead(analogChannel);
          myClient.print("analog input ");
          myClient.print(analogChannel);
          myClient.print(" is ");
          myClient.print(sensorReading);
          myClient.println("<br />");     
        }
    }
    
    void loop ()
    {
    // listen for incoming clients
      EthernetClient client = server.available();
      if (client) {
        Serial.println("new client");
        // an http request ends with a blank line
        boolean currentLineIsBlank = true;
        while (client.connected()) {
          if (client.available()) {
            char c = client.read();
            Serial.write(c);
            // if you've gotten to the end of the line (received a newline
            // character) and the line is blank, the http request has ended,
            // so you can send a reply
            if (c == '\n' && currentLineIsBlank) {
              // send a standard http response header
              client.print(headerHTML);
              // now send the stuff we want
              client.print(TimeElapsed()); // your old code here
              // do some more stuff
              sendAnalogToNetwork(client);
               // were done sending so now send the footer to close the page
              client.println(footerHTML);
              break;
            }
            if (c == '\n') {
              // you're starting a new line
              currentLineIsBlank = true;
            }
            else if (c != '\r') {
              // you've gotten a character on the current line
              currentLineIsBlank = false;
            }
          }
        }
        // give the web browser time to receive the data
        delay(1);
        // close the connection:
        client.stop();
        Serial.println("client disconnected");
      }
    }

     

    As you can see I have also provided a bit of re-formatting of the code to use more functions and variables for the constant strings, it could be better but it does demonstrate how the code needs to work on the Wiznet and also a few tips on program design

     

    I hope it meets your needs and gets you going int the right direction

     

    If this is the right Answer for you then please click "Correct Answer", thanks

    Attachments:
    RBBS_Server_Update.ino.zip