Arduino
  • Products
  • More
Arduino
Arduino Forum high frrequency PWM ,arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 2219 views
  • Users 0 members are here
  • arduino
Related

high frrequency PWM ,arduino

e14 Contributor
e14 Contributor over 12 years ago
High frequency PWM signal
Use and Arduino Uno microcontroller board to generate a variable frequency variable pulse with PWM signal .  The output pulse width should be adjustable , you can use an analog pin voltage varying from 0-5 V for duty cycle control (0 V should correspond to 0 duty cycle and  5V should correspond to 100% duty cycle).   The frequency of the signal should range from 10kHz to 20 kHz  and should be programmable .

i have a problem with the frequancy part, what i shloud do !
  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    there are a number of registers in the Atmega 328 that allow control of the duty cycle (Compare registers) and also pre-scale registers that will control crude frequency ranges (A division of the CPU clock (none, 2, 4, 8, 16, 32, 64)

     

    the two compare registers will control when the output goes high and low

     

    timer C can be configured to work in 16bit mode allowing more refined control of the output

     

    so one option is to use these registers to generate the output you need and allow the atmega to do other things

     

    the other option is to use the timer to create interrupts at the frequency you want and then have the interrupt routine directly change the output pin using a simple delay function to manage the pulse,

     

    A simple bit of math can factor for the pulse width to keep the frequency correct and to ensue the pulse width does not exceed the period of the frequency.

     

    based on this explanation I hope you can put a working sketch together, if not then post what you can get going and ill help more with some examples of my own that i will create to aid you.

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    CAN U PLZ GIVE ME  EXAMPLES THAT CAN HELP ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    Quick Response Day image

     

    I had a quick google, ended up on the actual Arduino Site and found this great article describing all sorts of PWM stuff including 16 Bit and fast PWM

     

    http://arduino.cc/en/Tutorial/SecretsOfArduinoPWM

     

    I hope it provides what you looking for