Arduino
  • Products
  • More
Arduino
Arduino Forum Help with coding Arduino for Adafruit Neopixels
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 20 replies
  • Subscribers 420 subscribers
  • Views 4022 views
  • Users 0 members are here
  • trinket
  • neopixel
  • ws2812
  • arduino
  • subroutine
Related

Help with coding Arduino for Adafruit Neopixels

funinalaska
funinalaska over 12 years ago

Ok, I am still struggling with coding issues.

I am trying to develop a subroutine (sorry for using the wrong term if that is incorrect but I do not know the proper terminology)

I am trying to program a trinket to control 4 Neopixel LEDs

I want to have the pixels turn on individually set to colors I choose using the strip.setPixelColor(n, R, B, G) code

Then I want to have them fade out using the strip.setBrightness(i) code and have "i" be a variable in the sub routine to run over and over fading from 255 (max brightness) to 0 (off) in increments assignable per step from 1 to 10

Then have the subroutine strip.setColorPixel(n, 0, 0, 0) and return i to 255 and then return to void loop for the next command

 

While I am at it, is there a way to have each of 4 neopixels fade at different times like have one pixel come on red and begin fading out and while that one is fading have another come on blue and start fading and then have the other 2 come on white then start fading. If not, i can handle them all fading at the same time, just curious

 

I can figure out how to have one LED come on and fade out then come back on and fade out in loop, but I don't know how to get this to work in a subroutine.

Thanks for any help.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +1
    I've just had a read through all of this and it was incredibly helpful as I'm doing something with neopixels that is very similar. Many thanks!
Parents
  • brett.lancaster
    0 brett.lancaster over 9 years ago

    Hey,

    terribly sorry for dragging up an old post!!

     

    im trying to use neo pixels my self for a project and ive run into an issue that i think is associated with the " delay(wait); " bit at the end. does any body know how to use milis() for example to get rid of the delay.

    or if its even possible to do so?

     

    thanks in advance!, Brett.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fvan
    0 fvan over 9 years ago in reply to brett.lancaster

    Not exactly sure what you mean, but for a use of "millis()", check the debounce example: https://www.arduino.cc/en/Tutorial/Debounce

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fvan
    0 fvan over 9 years ago in reply to brett.lancaster

    Not exactly sure what you mean, but for a use of "millis()", check the debounce example: https://www.arduino.cc/en/Tutorial/Debounce