Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Micro requires reset when powering on to boot properly
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1152 views
  • Users 0 members are here
  • keyboard
  • arduino-micro
  • arduino
  • booting
Related

Arduino Micro requires reset when powering on to boot properly

e14 Contributor
e14 Contributor over 12 years ago

Hi Everyone,

 

I followed the instructions here (https://learn.adafruit.com/usb-next-keyboard-with-arduino-micro?view=all) and got my NeXT keyboard to work with my Mac via the Arduino Micro and its Keyboard HID emulation. However, I have a strange issue. When I plug in the Arduino Micro to USB, the blue light on the bottom comes on but it doesn't attempt to boot until I push the reset button on the board. I tried writing a simple program that only sets LED 13 to High. When I uploaded that to the board, it boots normally. It does not require the reset and LED 13 lights up solid as the code requires. There must be something in the code provided by that project that causes it not to boot until its reset. I was wondering if anyone here could spot what might be causing my problem. I'll post the code before void loop() below. The rest of the code can be seen at this github project. (https://github.com/adafruit/USB-NeXT-Keyboard)

 

Thanks in advance for your help,

-Jeff

 

// NeXT non-ADB Keyboard to USB converter
// This will take an older NeXT keyboard, talk to it, and turn the keycodes into a USB keyboard
// Requires an Arduino Micro for the USB portion - but could be ported to another micro fairly easily
// Written by Limor Fried / Adafruit Industries
// Released under BSD license - thanks NetBSD! :)
//
// Timing reference thanks to http://m0115.web.fc2.com/
// Pinouts thanks to http://www.68k.org/~degs/nextkeyboard.html
// Keycodes from http://ftp.netbsd.org/pub/NetBSD/NetBSD-release-6/src/sys/arch/next68k/dev/


#include "wsksymdef.h"
#include "nextkeyboard.h"


// the timing per bit, 50microseconds
// I changed this to 51 as it seemed to make this more reliable. However, 51 broke the modifier keys.
#define TIMING 50


// pick which pins you want to use
#define KEYBOARDOUT 3
#define KEYBOARDIN 2


// comment to speed things up, uncomment for help!
//#define DEBUG


// speed up reads by caching the 'raw' pin ports
volatile uint8_t *misoportreg;
uint8_t misopin;
// our little macro
#define readkbd() ((*misoportreg) & misopin)


// debugging/activity LED
#define LED 13


#define NEXT_KMBUS_IDLE 0x200600


// NeXT Keyboard Defines
// modifiers
#define NEXT_KB_CONTROL 0x1000
#define NEXT_KB_ALTERNATE_LEFT 0x20000
#define NEXT_KB_ALTERNATE_RIGHT 0x40000
#define NEXT_KB_COMMAND_LEFT 0x8000
#define NEXT_KB_COMMAND_RIGHT 0x10000
#define NEXT_KB_SHIFT_LEFT 0x2000
#define NEXT_KB_SHIFT_RIGHT 0x4000


// special command for setting LEDs
void setLEDs(bool leftLED, bool rightLED) {
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING *9);
  digitalWrite(KEYBOARDOUT, HIGH);  
  delayMicroseconds(TIMING *3);
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING);


  if (leftLED)
      digitalWrite(KEYBOARDOUT, HIGH);
  else 
      digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING);


  if (rightLED)
      digitalWrite(KEYBOARDOUT, HIGH);
  else 
      digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING);
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING *7);
  digitalWrite(KEYBOARDOUT, HIGH);
}


void query() {
  // query the keyboard for data
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING *5);
  digitalWrite(KEYBOARDOUT, HIGH);  
  delayMicroseconds(TIMING );  
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING *3);
  digitalWrite(KEYBOARDOUT, HIGH); 
}


void nextreset() {
  // reset the keyboard
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING);
  digitalWrite(KEYBOARDOUT, HIGH);  
  delayMicroseconds(TIMING*4);  
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING);
  digitalWrite(KEYBOARDOUT, HIGH);
  delayMicroseconds(TIMING*6);
  digitalWrite(KEYBOARDOUT, LOW);
  delayMicroseconds(TIMING*10);  
  digitalWrite(KEYBOARDOUT, HIGH);
}




void setup() {
  // set up pin directions
  pinMode(KEYBOARDOUT, OUTPUT);
  pinMode(KEYBOARDIN, INPUT);
  pinMode(LED, OUTPUT);
  
  misoportreg = portInputRegister(digitalPinToPort(KEYBOARDIN));
  misopin = digitalPinToBitMask(KEYBOARDIN);
  
  // according to http://cfile7.uf.tistory.com/image/14448E464F410BF22380BB
  query();
  delay(5);
  nextreset();
  delay(8);
  
  query();
  delay(5);
  nextreset();
  delay(8);
  
  Keyboard.begin();


#ifdef DEBUG
  while (!Serial)
  Serial.begin(57600);
  Serial.println("NeXT");
#endif
}


uint32_t getresponse() {
  // bitbang timing, read 22 bits 50 microseconds apart
  cli();
  while ( readkbd() );
  delayMicroseconds(TIMING/2);
  uint32_t data = 0;
  for (uint8_t i=0; i < 22; i++) {
      if (readkbd())
        data |= ((uint32_t)1 << i);
      delayMicroseconds(TIMING);
  }
  sei();
  return data;


}

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 12 years ago

    Jeff

    I'm wondering if the Arduino is looking for serial data and thinking that its a download.

    I'm not the expert on the bootloader and I recall some discussion over at arduino.cc some time back.

     

    You didn't say which Arduino you had, and some have newer bootloaders programmed.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    Hi Mark,

     

    Thanks for the reply. The board I'm using is an Arduino Micro (http://arduino.cc/en/Main/ArduinoBoardMicro). Its an ATmega32u4.

     

    Do you think it could be waiting for serial data? How can I get it to stop doing that?

     

    -Jeff

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    Jeffrey

    It looks the same board and setup.

     

    It might be getting hung during the USB enumeration.

    You could try adding a delay(1000) in the void setup() to effectively make it pause trying to run the program for 1 second.

     

    The only other suggestion is post some feedback to Adafruit as it could be something specific to the USB and the MAC.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    Mark!

     

    You're a lifesaver! 1000 ms delay right after void setup() did it! It boots up without issues now. I was able to lower it to 500ms and get the same results. When I set it to 250, it would still freeze when plugged in.

     

    Thanks so much for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    Mark!

     

    You're a lifesaver! 1000 ms delay right after void setup() did it! It boots up without issues now. I was able to lower it to 500ms and get the same results. When I set it to 250, it would still freeze when plugged in.

     

    Thanks so much for your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    Jeffery.

    Well done, you passed very good information with links to the sources making it easier.

     

    Can I suggest that you feed this back to Adafruit, in case someone else is looking for the same solution/problem.

     

    Thanks

    Mark