Arduino
  • Products
  • More
Arduino
Arduino Forum ShiftPWM, and the TLC5940 with High Power LEDs?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 415 subscribers
  • Views 328 views
  • Users 0 members are here
  • lighting
  • pwm
  • tlc5940
  • led
  • shiftpwm
Related

ShiftPWM, and the TLC5940 with High Power LEDs?

funinalaska
funinalaska over 12 years ago

I found this on Sparkfun

https://www.sparkfun.com/products/10136

And somewhere I remembered reading that this chip has been used to control 1W 350ma high power LEDs

I think what they were doing was connecting each LED up to 3 outputs of this driver.

Would this work??

Can someone help me out with the possibility of doing this?

Also, Would I be better off using the above chip

or this board:

https://www.sparkfun.com/products/10616

I don't think I would need the regulator on the board if I used just the chip as I will already be using regulated 5V power supply

And I can add the capacitors easily enough

 

Will I have a problem with heat using either of these methods?

 

If I understand this correctly All I need external hardware besides my LEDs are a 0.1uF Capacitor and my Iref resistor.

If I set my Iref with a 360 ohm resistor that will give me an output of 108.5mA output per pin

my leds are 300-350mA LEDs so if I use 3 pins per LED that is 325.5mA which should be sufficient.

 

Also if doing this, when dimming should all 3 outputs per LED me in sync or would I be better off using them as staged dimmers?

 

Also, a curiosity question if any cares to answer, what would someone recommend as the maximum wire length between the Arduino control board and the TLC IC?

If possible I would like to be able to locate these "dimmer" modules in different locations and the closest to the Arduino would be greater than 9 feet (3 meters)

 

Thanks for the help  from anyone that can.