Arduino
  • Products
  • More
Arduino
Arduino Forum Xbee's to control quad copter?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 335 views
  • Users 0 members are here
  • diy
  • Design
  • arduino
Related

Xbee's to control quad copter?

gtrplyer16
gtrplyer16 over 12 years ago

     I am starting to design a quadcopter, however, I was curious if I could (with somewhat ease) do it purely using an Arduino using different shields. Or if anyone has done it before could you please share what you have discovered and pictures if you could!

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 12 years ago +1
    I have not done it that way purely because when you start building one of these, the functionality just expands as you move along the project. For a basic QC, you need the arduino to talk to electronic…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Yes to communicate between arduino and QC's remote control xbee is a best choice. a problem with using arduino at QC side is "balancing" . balancing can be maintain by choosing proper frame of QC and placing…
Parents
  • ipv1
    0 ipv1 over 12 years ago

    I have not done it that way purely because when you start building one of these, the functionality just expands as you move along the project. For a basic QC, you need the arduino to talk to electronic speed controls for the four rotors and sensors like Gyros, accelerometers and optionally magnetometers. The sensor data is fused via a kalman filter and the stability is maintained by a PID control routine. After that you can control it using what not like IR remote or RF remotes(better) or RF links to a laptop application like with an XBEE.

     

    You can write serial commands to control the quadcopter and then have a GUI on your laptop that sends commands over serial for the same.

    Its doable!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ipv1
    0 ipv1 over 12 years ago

    I have not done it that way purely because when you start building one of these, the functionality just expands as you move along the project. For a basic QC, you need the arduino to talk to electronic speed controls for the four rotors and sensors like Gyros, accelerometers and optionally magnetometers. The sensor data is fused via a kalman filter and the stability is maintained by a PID control routine. After that you can control it using what not like IR remote or RF remotes(better) or RF links to a laptop application like with an XBEE.

     

    You can write serial commands to control the quadcopter and then have a GUI on your laptop that sends commands over serial for the same.

    Its doable!