Arduino Forum I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?
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
  • State Not Answered
  • Replies 21 replies
  • Subscribers 405 subscribers
  • Views 4513 views
  • Users 0 members are here
Related

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?

Former Member
Former Member over 11 years ago

Hi,

 

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it? I would use two ultrasonic sensor to measure the difference of transmit time to calculate the air flow velocity. So I also want to know which circuit / circuit diagram I can use to connect between the ultrasonic sensors and the Arduino board. 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to Former Member +1
    Kelvin, suppose your tube is 15cm diameter and the spacing between the transducers along the tube is 20cm (sounds OK for a cooker hood chimney). The path length will be 36cm so the sound will take v. approx…
Parents
  • michaelwylie
    0 michaelwylie over 11 years ago

    I'm not sure about the Arduinos, but I have done this exact project for a senior design class. I used a PIC microcontroller. You're probably looking at 40 kHz transducers? Seriously here, do not get the hermetically sealed transducers, the received signal strength will be significantly lower and you'll have to deal with noise issues. If I recall correctly I had a 4 stage Butterworth filter in the final design and it was still finicky, all because of the very low signal levels from the sealed transducers.

     

    Are you going for a single TX to RX configuration, or are you going to array the sensors for a directional result? I.e are you measuring wind speed or velocity? The sensors I used were mounted in a triangle and were about 10 - 15 cm apart.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to michaelwylie

    Hi Michael,

     

    Thank you for your useful information. I want to make an airflow meter to measure the flow rate of air conditioner or range hood. My idea is to use two ultrasonic transducers clamped on a tube of diameter varied from 10 - 30cm and the transducers are mounted in V method. You are right, 40kHz transducers seem appropriate. It is the beginning of my project. I have many problems to solve. 

     

    • Two ultrasonic transducers will be used transceivers to transmit and receive ultrasound alternatively to measure the difference of transit time ( upstream and downstream ), and hence the airflow velocity. The flow rate is velocity times cross section area of the tube. However, I cannot find the circuit diagram of multiplexer for this purpose. I don't know how to obtain the transit time of upstream and downstream ( Tup & Tdn ).
    • If the Tup and Tdn can be obtained, how can I use the microcontroller to convert this data and the tube perimeter into the flow rate to be displayed in a LCD panel. I don't know MCU programming well. I heard that Arduino is more easy to learn.

     

    Could you share some more information of your ultrasonic airflow meter in detail?

     

    Regards,

    Kelvin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to michaelwylie

    The " V " method is shown in the image. You are right. If two measurements ( differential transmit time ) is used, the speed of sound can be eliminated and hence the temperature from the equation. What circuit I can use to pulse the transducer and receive the return pulse alternatively and calculate the differential transmit time before input into MCU.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 11 years ago in reply to Former Member

    What values of times do you want to measure? Tens of microseconds? Milliseconds?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to michaelwylie

    Do these Ultrasonic systems offer much greater accuracy than the heated element types like cars use for the MAF sensors?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to Former Member

    Kelvin, suppose your tube is 15cm diameter and the spacing between the transducers along the tube is 20cm (sounds OK for  a cooker hood chimney). The path length will be 36cm so the sound will take v. approx 0.36/300 = 1.2mS.

    A typical (first one I found with a spec) cooker hood moves 486cubic meters of air per hour = 0.135 per second. The area of the 15cm tube is 0.017 m^2 so the air velocity is 7.6m/s.

    Only 20/36 of you path is speeded up by the air moving so the difference in times will be 1.2mS*(15.2/300)*20/36 = 33.7 uS.

    If you use a 40kHz transducer each cycle takes 25uS so your full scale sensitivity is 1 sensor cycle time.

    You will need to estimate the transit time to within less than 1uS - which will be very very difficult and impossible without additional (to an Arduino) hardware.

     

    Here is a link to a commercial instrument, they use transducers at frequencies from 500kHz to 8MHz.

     

    FLUXUSRegistered F601 - The Portable Multi-Functional Flowmeter | FLEXIM

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to michaelkellett

    Here's a link to a Maxim chip with lots of info:

     

     

    http://datasheets.maximintegrated.com/en/ds/MAX35101.pdf

     

    In the first paragraph:

     

    With a time measurement accuracy of 20ps and automatic

    differential time-of-flight (TOF) measurement, this

    device makes for simplified computation of liquid flow.

    Early edge detection ensures measurements are made.........

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to michaelkellett

    Good one Michael, It shows that it's the right sensing you should be focusing on rather than the processing.

     

    Kelvin, is there a budget for this I'm sure some of these fine devices are outside a small project budget  ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to michaelkellett

    and the chip is only 15$ one off, it sounds expensive till you realize it supports the temperature measurement and compensation too which is essential for accurate measurement

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    That's not bad for what it's doing Peter, Did you find a price for the sensors as well?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Problemchild

    I did not, I was assuming that you could use some of the basic transducers from E14 or EBay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    I think this is the key think to be looking at for his design the CPU is pretty secondary to the Sensor and electronics sid.

    Would be nice if the cheap ones work OK though! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    I think this is the key think to be looking at for his design the CPU is pretty secondary to the Sensor and electronics sid.

    Would be nice if the cheap ones work OK though! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to Problemchild

    short of getting samples it would not be easy to tell

     

    I can get sample chip from TI without an issue as my business is registered with them, I would just have to get sensors and time image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to Robert Peter Oakes

    Yep back to the toy factory.