Arduino
  • Products
  • More
Arduino
Arduino Forum I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 420 subscribers
  • Views 5440 views
  • Users 0 members are here
Related

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it? I would use two ultrasonic sensor to measure the difference of transmit time to calculate the air flow velocity. So I also want to know which circuit / circuit diagram I can use to connect between the ultrasonic sensors and the Arduino board. 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    Kelvin, suppose your tube is 15cm diameter and the spacing between the transducers along the tube is 20cm (sounds OK for a cooker hood chimney). The path length will be 36cm so the sound will take v. approx…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Do you know what range of time will be involved

     

    this would be the time from the outbound ping to the sensor on the other end receiving it (Based on distance and air velocity)

     

    with this info you can better narrow down what kind of performance you will need from the system and therefore identify the right controller type

     

    are you reflecting the ultrasonic ping back to the same place as it was sent or having separated receiver and transmitter

     

    what transducers are you going to use ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    Do you know what range of time will be involved

     

    this would be the time from the outbound ping to the sensor on the other end receiving it (Based on distance and air velocity)

     

    with this info you can better narrow down what kind of performance you will need from the system and therefore identify the right controller type

     

    are you reflecting the ultrasonic ping back to the same place as it was sent or having separated receiver and transmitter

     

    what transducers are you going to use ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 12 years ago in reply to Robert Peter Oakes

    Have a look at the links I posted here.

    http://www.element14.com/community/groups/internet-of-things/blog/2014/04/13/impact-vibration-and-ultrasound-sensing-with-pvdf-piezo-sensors#comment-33459

     

    Vaisala have published much of the information you probably want to know.

     

    Mark