Arduino Forum I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?
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
  • State Not Answered
  • Replies 21 replies
  • Subscribers 405 subscribers
  • Views 4502 views
  • Users 0 members are here
Related

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?

Former Member
Former Member over 11 years ago

Hi,

 

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it? I would use two ultrasonic sensor to measure the difference of transmit time to calculate the air flow velocity. So I also want to know which circuit / circuit diagram I can use to connect between the ultrasonic sensors and the Arduino board. 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to Former Member +1
    Kelvin, suppose your tube is 15cm diameter and the spacing between the transducers along the tube is 20cm (sounds OK for a cooker hood chimney). The path length will be 36cm so the sound will take v. approx…
Parents
  • Former Member
    0 Former Member over 11 years ago

    Hi Kelvin,

     

    What arduino board and sensors did you end up using?

     

    I am working on a similar project to measure breathing.

     

    For now I was thinking on placing two SRF05 sensors on opposite sides of a tube (diagonal in the tube).

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Hi Kelvin,

     

    What arduino board and sensors did you end up using?

     

    I am working on a similar project to measure breathing.

     

    For now I was thinking on placing two SRF05 sensors on opposite sides of a tube (diagonal in the tube).

     

    Thanks!