Arduino
  • Products
  • More
Arduino
Arduino Forum I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 420 subscribers
  • Views 5446 views
  • Users 0 members are here
Related

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

I want to make an ultrasonic air flow meter. Which Arduino board is suitable for it? I would use two ultrasonic sensor to measure the difference of transmit time to calculate the air flow velocity. So I also want to know which circuit / circuit diagram I can use to connect between the ultrasonic sensors and the Arduino board. 

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to e14 Contributor +1
    Kelvin, suppose your tube is 15cm diameter and the spacing between the transducers along the tube is 20cm (sounds OK for a cooker hood chimney). The path length will be 36cm so the sound will take v. approx…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    The problem you both may face is the time between the pulse out and the response being detected, I have worked with ultrasonic flow meters in the past but they where on gas pipeline measuring a meter in diameter

     

    if your pipe is only an inch or so you may not have much resolution on the measurement, without doing the math the speed of sound and the distance will give you an idea of the timing, an arduino running at 16Mhz may not be able to capture the events with much accuracy (Most of the ultrasonic sensors do not resolve mm accuracy so external hardware may be necessary or atleast the use of actual machine/assembly code on the micro

     

    Regards

     

    peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    The problem you both may face is the time between the pulse out and the response being detected, I have worked with ultrasonic flow meters in the past but they where on gas pipeline measuring a meter in diameter

     

    if your pipe is only an inch or so you may not have much resolution on the measurement, without doing the math the speed of sound and the distance will give you an idea of the timing, an arduino running at 16Mhz may not be able to capture the events with much accuracy (Most of the ultrasonic sensors do not resolve mm accuracy so external hardware may be necessary or atleast the use of actual machine/assembly code on the micro

     

    Regards

     

    peter