Arduino
  • Products
  • More
Arduino
Arduino Forum How to Recreate a mV signal?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 415 subscribers
  • Views 986 views
  • Users 0 members are here
Related

How to Recreate a mV signal?

matt.wellsite
matt.wellsite over 12 years ago

I'm working on a project with an 2 Arduino's to transmit a load-cell's signal. I'm very new but fell I have an understanding enough for this project except for the last part.


I plan on using an op amp to boost the signal into the first Arduino but need to get the second to bring the signal back to it's original mV form, so really the question I have is what component to do this with?


The load-cells specs:

     Operating range:     0 to 50,000 lbs

     Input Voltage:          5 VDC

     Zero Offset:              0 mV at zero load

     Output Voltage:        2 mV/V ±1% at rated load


The loadcells output is 2 mVDC of excitation at full load of 50,000 lbs, my signal voltage will be somewhere between 0 and 10 mVDC.


So this doesn't fully apply to Arduino but this is the only place I could think to post my question.

Thanks for any and all help

Matt

  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago

    Amplifiers and excitation for load cells is  a complicated topic. You haven' specified enough to comment on the kind of approach you will need.

     

    The additional information required is:

    maximum error permitted in measurement

    measurement intervals e in 50000 lbs (often 1500,3000 or 6000)

    response time

    working temperature range

    are there any legal or safety implications

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago

    An arduino can provide an analog output 2 ways:

    1. by generating a PWM output (using the analogWrite() function) which is then filtered externally to create an analog signal.
    2. by digital-to-analog converter (on an arduino Due) also using analogWrite()

    To reduce the voltage all you need is a pair of resistors connected as a voltage divider or a potentiometer. The resulting low level signal could be buffered with a voltage follower op-amp to simulate the low impedance of the original load cell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer