Ok, so again, I didn't pay thorough enough attention to the item I was purchasing when I ordered something from ebay.
I ordered this:
http://www.ebay.com/itm/301129164770?ssPageName=STRK:MEWNX:IT&_trksid=p3984.m1439.l2649
Thinking it was this:
https://www.adafruit.com/products/326
Both units use the SSD1306 IC driver
But the one from Ada has more connection pins.
I am confused because all of the examples and instructables I can find that connect these using I2C use an additional pin for reset.
This unit does not have the reset pin only VCC, GND, SCL and SDA
The other thing is in the description it states that the screen is compatible with 3-5V
Should I assume that it is ready for 5v for VCC as well as signal or should I plan on using a logic level converter?
I bought this as a simple and cheap solution to a small display for network of temperature sensors that are going around an RV.
I am not looking to be able to display graphics only text. I would like to be able to get 3-4 lines of text on this little screen if I can.
It's funny how what you think will be the simple solution never really is.