Arduino Forum Arduino Mega + GPRS shield serial communication
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 402 subscribers
  • Views 1444 views
  • Users 0 members are here
  • mega
  • v1.1
  • sim900
  • icomsat
  • gprs
  • serial
  • 2560
  • arduino
  • communication
Related

Arduino Mega + GPRS shield serial communication

ivars88
ivars88 over 11 years ago

Hello!

Im having difficulties reading data from SIM900 module.

I am using IComSat v1.1 - SIM900 GSM/GPRS shield for Arduino modul and connecting it to Arduino MEGA. 19 pin(RX1) of Arduino i connect with moduls TX7 and Arduino 18 pin(TX1) with RX7. Below is the picture showing it.

http://www.bildites.lv/images/0jjlmdpljb2o79p0c3d2.jpg

 

 

 

Dont worry about power, i also used 72VA power supply, it didnt worked also. Modem doesnt need such current as recomennded for serial communication.

Tx from Arduino works because i can make call and send sms, but in serial port monitor i cant see no data coming from SIM900.

 

 

As im not sure there's a problem in programm or hardware i added my sketch below. Basically there is 4 cases - 2nd case calls and hangs up, in 3rd im asking is there any sms and in 4th case im asking signal quality. In 3rd and 4th case atleast something needs to be showing in serial port monitor but nothing..

 

 

I also used lines like this for data reading from SIM900, but none of them worked.

if (mySerial.available())

{

   Serial.write(mySerial.read());

}

 

 

if (mySerial.available() > 0)

{

  Serial.println(mySerial.read());

}

 

 

if(mySerial.available() >0)

  {

    incoming_char=mySerial.read(); //Get the character from the cellular serial port.

    Serial.print(incoming_char); //Print the incoming character to the terminal.

  }

}

 

 

Complete code:

 

#include <SoftwareSerial.h>

 

 

SoftwareSerial mySerial(19, 18);  //Arduino 18 pin(TX1) and 19 pin(RX1)

 

 

int LED = 13;

 

 

void setup()

{

pinMode(LED, OUTPUT);

Serial.begin(19200);

mySerial.begin(19200);  // the GPRS baud rate

powerUp();

 

}

 

void powerUp()

{

pinMode(9, OUTPUT);

digitalWrite(9,LOW);

delay(1000);

digitalWrite(9,HIGH);

delay(2000);

digitalWrite(9,LOW);

delay(9000);

Serial.println("Modem powered");

}

 

void loop()

{

  if (Serial.available())

  {

    char inSer = Serial.read();

    switch (inSer)

    {

      case '1':      //Just for confirmation that incoming characters from serial port is reading

      digitalWrite(LED, HIGH);

      delay(3000);

      digitalWrite(LED, LOW);

      break;

 

      case '2':

      mySerial.println("ATD + +371200....;"); //Calling to my cell. I just deleted part of my phone number cus i dont want to shove it

      delay(100);

      mySerial.println();

      delay(7000);       

      mySerial.println("ATH");  //Hangup

      break;

 

      case '3':

      mySerial.println("AT+CNMI=?\r");  //asking for new sms message indication

      delay(100);

      break;

 

      case '4':

      mySerial.println("AT+CSQ=?\r");  //asking for signal quality report

      delay(100);

      break;

    }

  }

if (mySerial.available())

{

   Serial.write(mySerial.read());

}

}

 

 

 

I would be appreciated for help how to read data from SIM900 image

  • Sign in to reply
  • Cancel

Top Replies

  • theenggprojects
    theenggprojects over 10 years ago in reply to Former Member +1
    I think you should check this one out http://www.theengineeringprojects.com/2014/06/send-sms-with-arduino-uno-and-sim900d-using-at-commands.html They have explained in detail how to send sms with sim900D…
Parents
  • Former Member
    0 Former Member over 10 years ago

    Hi.

     

    I've been struggling with this one too. Even resorted to using Hardware serial, instead of sofware serial, using serial1, 18 &19 of the mega, from 1 & 2 of the Gsm/GPRS shield. switching the jumpers to Xduino on the shield. but I seem to be reading random data, although it shows that it has received an sms when I send it an sms on the serial monitor. I fail to output the sms on the serial monnitor.

     

    Maybe together we can strike some success.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theenggprojects
    0 theenggprojects over 10 years ago in reply to Former Member

    I think you should check this one out http://www.theengineeringprojects.com/2014/06/send-sms-with-arduino-uno-and-sim900d-using-at-commands.html

     

    They have explained in detail how to send sms with sim900D using arduino via AT commands, plus also have alook on this link http://www.theengineeringprojects.com/2015/02/receive-sms-commands-using-sim900-arduino.html ..... In the firsst link its given in detail how to send sms while in the second link it shown how to receive sms so I think combining both will solve the problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • theenggprojects
    0 theenggprojects over 10 years ago in reply to Former Member

    I think you should check this one out http://www.theengineeringprojects.com/2014/06/send-sms-with-arduino-uno-and-sim900d-using-at-commands.html

     

    They have explained in detail how to send sms with sim900D using arduino via AT commands, plus also have alook on this link http://www.theengineeringprojects.com/2015/02/receive-sms-commands-using-sim900-arduino.html ..... In the firsst link its given in detail how to send sms while in the second link it shown how to receive sms so I think combining both will solve the problem.