Arduino
  • Products
  • More
Arduino
Arduino Forum LCD ARDUION PROGRAM QUERY
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 411 views
  • Users 0 members are here
Related

LCD ARDUION PROGRAM QUERY

e14 Contributor
e14 Contributor over 12 years ago

Hi guys i have built an two pir sensor arduino program that will turn the leds.Now i want to connect the LCD AS WEL..

I WANT TO MAKE 4 BITS ARDUINO LCD PROGRAM.I have made this program as show below.When the Button pin 1 will activate it will turn on led 1 and lcd will show "motion detected" for 2 seconds .And when button pin 2 will activate it will show same for 2 seconds.

I am using 16X2 pin Lcd.


I could not how to make the void loop of this program.Any help guys or any basic program if u can make.i will realy appreciate that.thanks

 

 

const int buttonPin1 = 2;     // the number of the pushbutton pin 2

const int buttonPin2 = 3;     // the number of the pushbutton pin 3

const int ledPin1 =  13;      // the number of the LED pin

const int ledPin2 =  12;

// variables will change:

int buttonState1= 0;         // variable for reading the pushbutton status

int buttonState2= 0;

 

void setup() {

  // initialize the LED pin as an output:

  pinMode(ledPin1, OUTPUT);  

  pinMode(ledPin2, OUTPUT);

  // initialize the pushbutton pin as an input:

  pinMode(buttonPin1, INPUT);

  // initialize the pushbutton pin as an input:

  pinMode(buttonPin2, INPUT);  

}

 

 

void loop(){

  // read the state of the pushbutton value:

  buttonState1 = digitalRead(buttonPin1);

  // read the state of the pushbutton value:

  buttonState2= digitalRead(buttonPin2);

 

 

  // check if the pushbutton is pressed.

  // if it is, the buttonState is HIGH:

  if (buttonState1 == HIGH) {   

    // turn LED on:  

    digitalWrite(ledPin1, HIGH);

    delay(1000);

    digitalWrite(ledPin2, LOW);

    delay(1000);

  if

     (buttonState2 == HIGH) {   

    // turn LED on:  

    digitalWrite(ledPin2, HIGH);

    delay(1000);

    digitalWrite(ledPin1, LOW);

    delay(1000);

  }

  }

 

 

}

 

Attachments:
sketch_may13f.ino.zip
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    here you go

     

    http://arduino.cc/en/Tutorial/LiquidCrystal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    thats very simple program,how to use the if statment in loop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    thats very simple program,how to use the if statment in loop