Arduino
  • Products
  • More
Arduino
Arduino Forum What should I buy?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 533 views
  • Users 0 members are here
  • raspberry
  • rover
  • kali
  • arduino
  • quadcopter
Related

What should I buy?

e14 Contributor
e14 Contributor over 12 years ago

Hello everyone,

I have a project idea as follows:

My laptop connects to a mobile embedded device which is capable of communicating with the network.

After some searching I found out that you can ssh into a raspberry pi and execute commands on it like on the localhost.

I need a raspberry pi because I want to install kali linux on it for you know why.

To make it more fun I want to add a mobile component a rover or maybe a quad-copter depending on the budge(I'll prefer the cheaper one image).

Searching further has resulted in a confusion of rovers being built mostly on arduino.

So do I need both of them to achieve the task i.e. A RC controls arduino-rover and I ssh into kali on my pi?

Kindly guide me to a simpler implementation of my idea as to what components I'll be needing.

Thanking you,

Srikanth

  • Sign in to reply
  • Cancel
  • dougw
    0 dougw over 12 years ago

    The Raspberry Pi needs an interface card to connect to motors and sensors in a vehicle.

    One solution is to use a ChipKit Pi which plugs into a Raspberry Pi and provides an arduino compatible interface for peripherals. This is a high performance arduino compatible solution that allows use of available arduino sketches and can be programmed via the RPi.

     

    chipKITTm Pi - The latest ArduinoTm compatible chipKITTm platform from Microchip and element14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Thanks for replying it was very helpful.