Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sensor to detect Human Presence
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 81 replies
  • Answers 34 answers
  • Subscribers 442 subscribers
  • Views 16758 views
  • Users 0 members are here
  • human
  • detection
  • internet_of_things
  • arduino
  • sensor
Related

Sensor to detect Human Presence

gunaseelan
gunaseelan over 12 years ago

Hello Friends,

 

                    Is there any sensor to detect human presence . Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence . Another way is by using image processing technique. Kindly suggest me a better solution image .

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +7 suggested
    Hi Gunaseelan, OMRON do a thermal sensor that can detect stationary thermal objects as opposed to standard PIR motion sensor that only detect motion. The OMRON D6T thermal sensor is able to detect the…
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz +6 suggested
    shabaz Voight-Kampff machine ? Voight-Kampff machine | Off-world: The Blade Runner Wiki | FANDOM powered by Wikia
  • shabaz
    shabaz over 7 years ago in reply to dougw +5 suggested
    Agree.. I don't know why the OP excludes image processing - due to incorrectly perceived difficulty, or for a non-technical reason. I can understand the desire to possibly exclude due to (say) security…
Parents
  • DAB
    0 DAB over 7 years ago

    You can use a thermal IR sensor calibrated to 98.6 degrees F and it will tell you when a human is in its field of view.

    You have to have the sensor at that precise temperature to discriminate between humans and animals. Just be aware that if someone is ill, they would not be detected.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • halimahext125
    0 halimahext125 over 6 years ago in reply to DAB

    I think that is a great start to answer the initial post @DAB. I think multiple IR sensors would be needed to detect the correct body temperature for human presence but also the size of the room and body form would need to be incorporated in my opinion. Will the sensor detect 98.6 degrees if someone first comes in the room? Maybe there will need to be a gauge on distance vs. temperature also. The further away the person is, will the IR sensor be able to determine between random heat or person? I think that ML will be able to solve the issue. I also think perhaps a picture can be taken with a motion detector hooked up to a camera to send an image and confirm that it is a presence there once the IR is set off. The initial post did come off as if there was a question of if there was a ghost there. Maybe i'm reading to much into that lolimage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • halimahext125
    0 halimahext125 over 6 years ago in reply to DAB

    I think that is a great start to answer the initial post @DAB. I think multiple IR sensors would be needed to detect the correct body temperature for human presence but also the size of the room and body form would need to be incorporated in my opinion. Will the sensor detect 98.6 degrees if someone first comes in the room? Maybe there will need to be a gauge on distance vs. temperature also. The further away the person is, will the IR sensor be able to determine between random heat or person? I think that ML will be able to solve the issue. I also think perhaps a picture can be taken with a motion detector hooked up to a camera to send an image and confirm that it is a presence there once the IR is set off. The initial post did come off as if there was a question of if there was a ghost there. Maybe i'm reading to much into that lolimage.