Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sensor to detect Human Presence
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 81 replies
  • Answers 34 answers
  • Subscribers 442 subscribers
  • Views 16790 views
  • Users 0 members are here
  • human
  • detection
  • internet_of_things
  • arduino
  • sensor
Related

Sensor to detect Human Presence

gunaseelan
gunaseelan over 12 years ago

Hello Friends,

 

                    Is there any sensor to detect human presence . Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence . Another way is by using image processing technique. Kindly suggest me a better solution image .

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +7 suggested
    Hi Gunaseelan, OMRON do a thermal sensor that can detect stationary thermal objects as opposed to standard PIR motion sensor that only detect motion. The OMRON D6T thermal sensor is able to detect the…
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz +6 suggested
    shabaz Voight-Kampff machine ? Voight-Kampff machine | Off-world: The Blade Runner Wiki | FANDOM powered by Wikia
  • shabaz
    shabaz over 7 years ago in reply to dougw +5 suggested
    Agree.. I don't know why the OP excludes image processing - due to incorrectly perceived difficulty, or for a non-technical reason. I can understand the desire to possibly exclude due to (say) security…
Parents
  • gsgill112
    0 gsgill112 over 8 years ago

    PIR sensor they are cheep and gets the job done !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to gsgill112

    Hi Gurinder, the OP specifically rules out PIR sensors:

    Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence .

    Anyway, I don't think a sensor exists to 'detect' humans, just some limited characteristics that humans have (and often these characteristics are not exclusive to humans either). Image recognition usually identifies anything that looks human-shaped. PIR detects anything warm that moves (cat or dog would be included). Also, plenty of 'human interaction' robots are designed to look and move like humans. They can speak too. Short of some intrusive surgery or extracting DNA, or interrogating and hoping that intelligent responses are present for only humans (and how long before this fails too?) I can't see how a machine or a sensor could 'detect' humans. Most of these characteristics can be faked too.

    This might sound pedantic but it's not any more, especially when cameras etc are used to unlock phones and PCs these days.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gsgill112
    0 gsgill112 over 8 years ago in reply to shabaz

    Correctly pointed out shabaz image I might have forgotten that while going through the comments, I agree , its difficult to figure out human presence if you are not using any kind of Thermal / Image sensing !

    Jee, sorry for the stupid comment image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to gsgill112

    Hi Gurinder,

     

    No worries, to be honest most of the comment was really for the OP anyway, since the question can't have a real answer without some significant bounds/limitations.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 8 years ago in reply to shabaz

    It's interesting to read through the comments as no one is focusing on the use of multiple sensor configurations to detect human presence. A single PIR certainly can't determine human movement from some other heat source movement but using multiple PIR sensors could.

     

    Imaging technology via a single lens configuration, for example, still only provides a 2 dimensional picture which does not always return the correct answer, so in my opinion, the ideal, more accurate, scenario would be to try and create a 3-d representation using multiple sensor types. Additional "dimensions" could include things like body mass, for example, which is a proven criteria to differentiate objects.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to BigG

    Hi! Indeed, times have changed, and a device can use processing and multiple sensors to get closer to extracting the desired knowledge of human presence.

    I forget the name, but there are commercial products that are used for unlocking doors, that use 3D information to detect facial features. I've seen one in action, you just have to stare into it for a couple of seconds.

    It shows the face on the screen but only for centering purposes, and instead it is measuring the distance to different features on the face. But I don't know if it can be fooled with something that is three-dimensionally like a human : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to shabaz

    Detecting humans is a big topic. Whoever wants to detect people needs to define the problem precisely if they are to have a hope of finding a suitable solution.

    • Cameras and image processing can easily detect people and even recognize who they are.
    • IR cameras have similar capabilities, but can see people in the dark.
    • MIR (micro-impulse radar) can detect heart beats or respiration even through walls.
    • FSR (force sensitive resistors) can measure footsteps and body weight.
    • IR thermometers can measure body temperature remotely (better than PIR).
    • Ultrasound can image people.
    • Xray scanners can see image people and their bones.
    • Millimeter wave scanners can image people and see through their clothing.
    • Microphones can detect breathing and footsteps.
    • People can be detected remotely by their charge or capacitance.
    • Human gas emissions like CO2 can be measured

    These are just off the top of my head - but there are obviously many technologies that can be used and fused.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rsc
    0 rsc over 8 years ago in reply to dougw

    Might be easier and cost effective to pay someone to stand there and watch for people.  People can usually detect other people.

    We use an ID card for meal tickets, and they are pre-paid, so if you go through the line twice, you get charged twice.

    Embedded NFC chips would work also.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rsc
    0 rsc over 8 years ago in reply to dougw

    Might be easier and cost effective to pay someone to stand there and watch for people.  People can usually detect other people.

    We use an ID card for meal tickets, and they are pre-paid, so if you go through the line twice, you get charged twice.

    Embedded NFC chips would work also.