Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Sensor to detect Human Presence
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 81 replies
  • Answers 34 answers
  • Subscribers 442 subscribers
  • Views 16779 views
  • Users 0 members are here
  • human
  • detection
  • internet_of_things
  • arduino
  • sensor
Related

Sensor to detect Human Presence

gunaseelan
gunaseelan over 12 years ago

Hello Friends,

 

                    Is there any sensor to detect human presence . Am aware of PIR (Passive Infra Red) sensor , which would human motion but not the human presence . Another way is by using image processing technique. Kindly suggest me a better solution image .

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +7 suggested
    Hi Gunaseelan, OMRON do a thermal sensor that can detect stationary thermal objects as opposed to standard PIR motion sensor that only detect motion. The OMRON D6T thermal sensor is able to detect the…
  • beacon_dave
    beacon_dave over 8 years ago in reply to shabaz +6 suggested
    shabaz Voight-Kampff machine ? Voight-Kampff machine | Off-world: The Blade Runner Wiki | FANDOM powered by Wikia
  • shabaz
    shabaz over 7 years ago in reply to dougw +5 suggested
    Agree.. I don't know why the OP excludes image processing - due to incorrectly perceived difficulty, or for a non-technical reason. I can understand the desire to possibly exclude due to (say) security…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi, I am trying to make an alarm system. What sensor can I use in detecting human presence outside the gate of a house and detects if someone is near their house?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi, I am trying to make an alarm system. What sensor can I use in detecting human presence outside the gate of a house and detects if someone is near their house?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Most intruder alarms use Passive Infrared detectors, that pick up on a rise of IR from a body - Good for about 10m (31ft) in optimal conditions.  These won't differentiate between a human and, say, a raccoon climbing on the gate.

    Depending upon what's outside the gate you could also use a motion detection system - That won't work if there's traffic close by the gate.  Motion detection is also commonly used within a perimeter.   The better detectors are capable of focused field and fairly long-range,  The lower-priced add-on boards are usually good to about 8m (25ft).

    I don't know what system you're using for a host, but there are common brands of these sensors on breakout or add-on boards for the most common microcontrollers and single-board computers.  High-end IP cameras also have motion-detection and alarm capability.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    yup, that pretty much covers it, you can also consider putting a magnetic switch on the gate itself as an additional measure to detect the intruder / visito or Laser / IR beams at strategic places, these could be high enough to avoid being tripped by smaller animals, they may trip for larger preditors like Bears and Sasquatch, or the odd moose image