Arduino
  • Products
  • More
Arduino
Arduino Forum project of arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 18 replies
  • Subscribers 419 subscribers
  • Views 1726 views
  • Users 0 members are here
Related

project of arduino

e14 Contributor
e14 Contributor over 12 years ago

i want the basic project of arduino with full programmming

  • Sign in to reply
  • Cancel

Top Replies

  • kidiccurus
    kidiccurus over 12 years ago +2
    This is the easiest project possible. Arduino - Blink
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    I am sorry but you need to provide a bit more detail of what you need help with Provide schematic, and or Code up to now, pictures, sketches etc. thanks
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to crosseyejack +1
    void setup() { pinMode(13, OUTPUT); } void loop() { digitalWrite(13,!digitalRead(13)); delay(1000); }
Parents
  • crosseyejack
    0 crosseyejack over 12 years ago

    Using the registers on the micro and compiling to 666 bytes. NICE :-)

     

    EDIT: Using _delay_ms(); we can get it down even smaller but I still like the 666 bytes compile

    #include <util/delay.h>
    void setup() {   
    DDRB = DDRB | B00100000; // set pin 13 to output     
    }  
    void loop() {  
      PORTB = PORTB ^ B00100000;
      _delay_ms(1000); 
    }

    Binary sketch size: 494 bytes (of a 32256 byte maximum, 1.53 percent).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to crosseyejack

    i looked for a lower level delay function but could not find it, well done image

     

    I will keep a mental note of that call for future

     

    As a beginner of course people will take the first approach but even in this simple demo is shows that when the memory starts to get constrained there are ways of significantly getting it back

     

    we reduced a >1234byte program by 2/3rds  (494 bytes) which is awesome if you think about it.

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to crosseyejack

    i looked for a lower level delay function but could not find it, well done image

     

    I will keep a mental note of that call for future

     

    As a beginner of course people will take the first approach but even in this simple demo is shows that when the memory starts to get constrained there are ways of significantly getting it back

     

    we reduced a >1234byte program by 2/3rds  (494 bytes) which is awesome if you think about it.

     

    Peter