Arduino
  • Products
  • More
Arduino
Arduino Forum project of arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 18 replies
  • Subscribers 419 subscribers
  • Views 1741 views
  • Users 0 members are here
Related

project of arduino

e14 Contributor
e14 Contributor over 12 years ago

i want the basic project of arduino with full programmming

  • Sign in to reply
  • Cancel

Top Replies

  • kidiccurus
    kidiccurus over 12 years ago +2
    This is the easiest project possible. Arduino - Blink
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    I am sorry but you need to provide a bit more detail of what you need help with Provide schematic, and or Code up to now, pictures, sketches etc. thanks
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to crosseyejack +1
    void setup() { pinMode(13, OUTPUT); } void loop() { digitalWrite(13,!digitalRead(13)); delay(1000); }
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    I am surprised we have not had comments regarding what we just did, Im sure there are plenty of new comers that are just shaking their head image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • crosseyejack
    0 crosseyejack over 12 years ago in reply to Robert Peter Oakes

    But its always fun to just mess about with code for just fun. Anyways it has been a while since I've played with Arduino's compiler but I've just had a quick 10 min play while waiting for something else to finish.

     

    While the first delay(1000); adds 190 bytes to the program every other delay(1000); only adds 12 bytes where each _delay_ms(1000); adds 18 bytes to the program so depending on how many delays you have in your program you might find its more efficient to use the Arduino delay(); over the AVR Libc _delay_ms(); A quick of the top of my head calculation would put that number around the 30 mark.

    void setup() {  
    DDRB = DDRB | B00100000; // set pin 13 to output    
    } 
    void loop() { 
      PORTB = PORTB ^ B00100000;
      delay(1000);
    }

    Binary sketch size: 666 bytes (of a 32256 byte maximum, 2.06 percent).

    void setup() {  
    DDRB = DDRB | B00100000; // set pin 13 to output    
    } 
    void loop() { 
      PORTB = PORTB ^ B00100000;
      delay(1000);
      delay(1000);
    }

    Binary sketch size: 678 bytes (of a 32256 byte maximum, 2.10 percent).

    void setup() {  
    DDRB = DDRB | B00100000; // set pin 13 to output    
    } 
    void loop() { 
      PORTB = PORTB ^ B00100000;
      delay(1000);
      delay(1000);
      delay(1000);
    }

    Binary sketch size: 690 bytes (of a 32256 byte maximum, 2.14 percent).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 12 years ago in reply to crosseyejack

    By easy, I did not mean short. Short helps, but sensible, easy to read code is just as important. Binary sketches are a little to difficult for a first project. When I made that post I didn't mean it as a challenge, but it's nice to see that you can do so much to such a simple program.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • crosseyejack
    0 crosseyejack over 12 years ago in reply to kidiccurus

    Yeah we got a little carried away with just messing around with code. Using digitalWrite(); is a lot simpler as the Arduino core handles all the bit handling and pin addressing for you. Sure on the ATMega328/168 DDRB = DDRB | B00100000; will set Arduino Pin 13 as an output but the Arduino is not just based around that ATMega. If you were using the Leonardo which is based around the ATMega32U4 pin 13 is actually C7 so if you wanted the same blink program running on the Leonardo you would have to change the code to:-

    void setup() {     
    DDRC = DDRC | B10000000; // set pin 13 to output       
    }    
    void loop() {    
      PORTC = PORTC ^ B10000000;  
      _delay_ms(1000);
    }

    Which isn't friendly to newcomers. digitalWrite(); gets rid of the headache and just handles all that for you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to crosseyejack

    That is an interesting observation, I would have expected the low level call to be better in all cases or certainly no worse after the first higher level call

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to crosseyejack

    That is an interesting observation, I would have expected the low level call to be better in all cases or certainly no worse after the first higher level call

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • crosseyejack
    0 crosseyejack over 12 years ago in reply to Robert Peter Oakes

    But you can get even smaller than _delay_ms(); and pretty efficient for the simple tests we are doing

     

    void setup() {     
    DDRB = DDRB | B00100000; // set pin 13 to output       
    }    
    void loop() {    
      PORTB = PORTB ^ B00100000;  
      delnms(1000);   
    }  
    
    void delnms(unsigned int n){ 
    //delay n ms 
    unsigned int x;
      while(n--){ 
        x=2600;       //empirically determined fudge factor 16mhz
        while(x--); 
      } 
    }

    Binary sketch size: 476 bytes (of a 32256 byte maximum, 1.48 percent).

    Source: View topic - AVR Delay Functions :: AVR Freaks

     

    void setup() {     
    DDRB = DDRB | B00100000; // set pin 13 to output       
    }    
    void loop() {    
      PORTB = PORTB ^ B00100000;  
      delnms(1000);   
      delnms(500);   
      delnms(1000);   
    }  
    
    void delnms(unsigned int n){ 
    //delay n ms 
    unsigned int x;
      while(n--){ 
        x=2600;       //empirically determined fudge factor 16mhz
        while(x--); 
      } 
    }

    Binary sketch size: 476 bytes (of a 32256 byte maximum, 1.48 percent).

    Yup even with more calls to the delay and even different delays didn't increase the compile size, but using this method can be a bit finicky. For example interrupts during the delay will cause the delay to increase in length.