Arduino
  • Products
  • More
Arduino
Arduino Forum Due Serial Port Rx0 Tx0. Rx0 appears to fail
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1180 views
  • Users 0 members are here
  • rx0
  • due
  • query
Related

Due Serial Port Rx0 Tx0. Rx0 appears to fail

e14 Contributor
e14 Contributor over 12 years ago

Hi I can show the Tx0 port working fine with Atmel Studio,Jtag and the Uart Example program. The receiver Rx0 remains high/virtually nchanging  when connected to an RS232 to 3.3V translator.

I have tried two boards with same result. Any guidance/experience with uart on Txo Rxo greatly appreciated.

Regards

        S Lawton

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    can you provide picture of your connectivity and also your code ?

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    1) The signal is generated via a PC via  Fedora19> Eclipse> Python> motion-driver- client> Keyboard strokes sent to the Serial port . The PC serial output is connected to an RS232 to 3.3v level translator. When the output from this device is open circuit the 3.3V side switches cleanly as char are sent.

    When connected to Rx0 on Due the signal hardly changes  (implying a short ?).

    2) The code is simply the build of the Atmel Uart Example program . I can prove the transmit side works fine but cannot see a fault (Yet!) in the Rx0 side eg PIO disconnect. Does this clarify?

    Thanks

               S Lawton

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    1) The signal is generated via a PC via  Fedora19> Eclipse> Python> motion-driver- client> Keyboard strokes sent to the Serial port . The PC serial output is connected to an RS232 to 3.3v level translator. When the output from this device is open circuit the 3.3V side switches cleanly as char are sent.

    When connected to Rx0 on Due the signal hardly changes  (implying a short ?).

    2) The code is simply the build of the Atmel Uart Example program . I can prove the transmit side works fine but cannot see a fault (Yet!) in the Rx0 side eg PIO disconnect. Does this clarify?

    Thanks

               S Lawton

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    I dont know you skill level or experiance so forgive this rather 101 statement

     

    Have you connected the RX of the adapter (Level Shifter) to the RX of the board, if so this is wrong, it should be RX to TX, TX to RX (Cross over so to speak)

     

    Are you accidentally using the pins on the controller for IO and setting them both to output ?

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Peter

    I will try a new path to cross check the electrical connection ( but the TX0 out does produce a signal generated from the Due code and it does appear on the output of the level shifter ). I will also review the example  board_init() keeping Tx, Rx directionality in view. Happy to receive your 101 as I cannot id bug thus far!

    Stewart  Lawton

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer