Arduino
  • Products
  • More
Arduino
Arduino Forum Due Serial Port Rx0 Tx0. Rx0 appears to fail
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 1181 views
  • Users 0 members are here
  • rx0
  • due
  • query
Related

Due Serial Port Rx0 Tx0. Rx0 appears to fail

e14 Contributor
e14 Contributor over 12 years ago

Hi I can show the Tx0 port working fine with Atmel Studio,Jtag and the Uart Example program. The receiver Rx0 remains high/virtually nchanging  when connected to an RS232 to 3.3V translator.

I have tried two boards with same result. Any guidance/experience with uart on Txo Rxo greatly appreciated.

Regards

        S Lawton

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I finally  found that the signal levels from the RS232 adapter appear to interfer ( observed on a CRT)  when powered from 3V3. On connecting the adapter to  5V and using

    http://www.ti.com/lit/ds/symlink/sn74lvc245a.pdf as level translators between the RS232 adapter and the Arduino due both TX and RX signals are available at the

    Arduino TX0 and RX0 (the silk screen arrows mark the signal direction to and from the Arduino pins respectively) . An inference is that the RS232 adapter voltage generator collapses at the lower PSU voltage.

    Hope this is helpful to others interfacing an old PC serial port, running Linux Fedora  to the Arduino Due via an RS232 adapter.

    S Lawton

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I finally  found that the signal levels from the RS232 adapter appear to interfer ( observed on a CRT)  when powered from 3V3. On connecting the adapter to  5V and using

    http://www.ti.com/lit/ds/symlink/sn74lvc245a.pdf as level translators between the RS232 adapter and the Arduino due both TX and RX signals are available at the

    Arduino TX0 and RX0 (the silk screen arrows mark the signal direction to and from the Arduino pins respectively) . An inference is that the RS232 adapter voltage generator collapses at the lower PSU voltage.

    Hope this is helpful to others interfacing an old PC serial port, running Linux Fedora  to the Arduino Due via an RS232 adapter.

    S Lawton