Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How to build the dagu rover 5 chassis with arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 3114 views
  • Users 0 members are here
  • hardware
  • diy
  • electrical
  • arduino
Related

How to build the dagu rover 5 chassis with arduino

nschreiber0813
nschreiber0813 over 12 years ago

Dear: Jeremy

I am building the dagu rover 5 chassis and I need your help. See I am trying to build a PCB for the dagu rover 5 chassis and I am running into a few problems. You see I looked at the dagu rover 5 datasheet and I am having trouble understanding it. I am really finding it broad and difficult to read due to my lack of engineering experience. Can you please help me because I can't figure out which wire goes to where and how due the encoders work. You can see the datasheet right here. Thank you.

From Noah

https://www.sparkfun.com/products/10336

http://dlnmh9ip6v2uc.cloudfront.net/datasheets/Robotics/RP6%20motor%20TFK280SC-21138-45.pdf

http://dlnmh9ip6v2uc.cloudfront.net/datasheets/Robotics/RP6%20motor%20TFK280SC-21138-45.pdf

image

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 4 years ago in reply to johan.seger +3
    This will depend upon the motor controller you are using and the version of the Dagu 5. It looks like it comes in 2 and 4 motor variants depending upon the tracked version or the mechanum wheeled version…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to nschreiber0813 +2 suggested
    I am glad you figured it out, thats always the best way to learn to help, you may find this interesting too Arduino Playground - RotaryEncoders these are actually switches that are great as a digital replacement…
  • colporteur
    colporteur over 4 years ago in reply to beacon_dave +2
    BD you're and encyclopedia of knowledge or you have a really good search engine:)
  • nschreiber0813
    0 nschreiber0813 over 12 years ago

    Dear: Element 14

    I liked to say first of all thank you for not responding to my post I actually figured out this problem on my own. Next thing you should know is that there are actually no tutorials on the internet for how to wire the rover 5 chassis to a homemade PCB. So anyways with hard endearing work I took apart my chassis and realized the brand of the encoder and found one greatly similar to it off the internet. Then you may be wondering what do all the wires mean. First of all there are four wires, red, black, yellow, and white. The white wire is channel A and the yellow wire is channel B. I am still not getting exactly how they work but I figured out that part. If you have and questions about my sources check the links bellow and thank you.

    From: Noah

    Rotary encoder - Wikipedia, the free encyclopedia

    US Digital | Products » E5 Optical Kit Encoder

    How to use a quadrature encoder | Let's Make Robots!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to nschreiber0813

    I am glad you figured it out, thats always the best way to learn

     

    to help, you may find this interesting too  Arduino Playground - RotaryEncoders

     

    these are actually switches that are great as a digital replacement for a pot and ADC on arduino etc. the bet thing is they use the same encoding methods you have linked in above so it can help you figureout the best way to read yours.

     

    Hope it is usefull

     

    Peter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johan.seger
    0 johan.seger over 4 years ago

    Hello im trying to build the dagu 5 with arduino and motor shield but don’t now how to connect the wires, and can’t find tutorials, do you have a intructubel?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 4 years ago in reply to johan.seger

    This will depend upon the motor controller you are using and the version of the Dagu 5. It looks like it comes in 2 and 4 motor variants depending upon the tracked version or the mechanum wheeled version. It also appears to come with 2 or 4 quadrature encoders.

    https://www.pololu.com/file/0J467/Rover%205.pdf  

    Looking at the photo, each motor has a red and black wire terminated in a large white connector. These need to be connected to your motor controller motor outputs. The bunch of four wires with individual black header sockets are the encoder connections which optionally can be connected to a quadrature decoder to give direction and speed information if you require it. The battery pack has a red and black wire and a smaller white connector. This is the 7.2V power supply for the motors and needs to be connected to the motor power input on the motor controller.

    Here is how it would look with the Arduino motor shield (only one motor shown as being connected):

    Arduino motor shield connections

    Image source linked from Arduino motor shield tutorial:
    https://docs.arduino.cc/tutorials/motor-shield-rev3/msr3-controlling-dc-motor

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 4 years ago in reply to beacon_dave

    BD you're and encyclopedia of knowledge or you have a really good search engine:)