Arduino
  • Products
  • More
Arduino
Arduino Forum Detect oscillations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 33 replies
  • Answers 1 answer
  • Subscribers 421 subscribers
  • Views 3525 views
  • Users 0 members are here
  • oscillations
  • processing
  • accelerometer
  • movement
  • algorithm
  • arduino
Related

Detect oscillations

kosme
kosme over 12 years ago

I'm trying to use an Arduino and a MMA8452Q accelerometer to sense movement and detect oscillations. What would be the best way to analyze and process the info to detect oscillations at a specific frequency range and act accordingly?

 

Edit 1:


Aswering Michael Kellett questions

Must you detect  a single frequency (known in advance) or a band of frequencies.

I must detect if the oscillation is in the 4-8Hz range.

 

Is the sampling rate under direct contorl of the Arduino or is it set by the accelerometer.

It is mostly under control of the Arduino. The accelerometer is set to sample at a certain rate but I can "miss steps" simply by reading the I2C interface at a much lower rate.

 

What is the range of frequencies and amplitudes you must detect.

I must detect if the oscillation is in the 4-8Hz range. The amplitude will be handled by the accelerometer but I expect it to be between ±4G's

 

Are there other signals present at the same time which you must ignore.

No, but it would be nice to be able to log the results.

 

How quickly must you reach a  decision when the signal appears.

I haven't decided that yet but the oscillation must persist for several seconds before action is taken. The exact number of seconds hasn't still been determined.

 

What accelerometer are you suing.

MMA8452Q I2C accelerometer

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago +1 suggested
    Hello Enrique, It makes it easier for people to follow the thread if you just add a new message rather than editing the original question. It seems that you want to detect energy in the band 4 - 8Hz, not…
  • D_Hersey
    D_Hersey over 12 years ago +1
    SO has just come down with Parky's, so I know of the characteristics of the tremors, they do seem to have a characteristic wave form, narrow fq, fairly constant amplitude between ramp-up and ramp-down…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Implement a mixer. A mixer takes an input signal at a known frequency and adds (or subtracts) its frequency value to your input signal. The maximum amplitude of the output signal will therefore correspond to the sum or difference of your two input signals. This way you detect the frequency and strength of the oscillations that you are looking for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago in reply to e14 Contributor

    Technically, to be a mixer, in this context, we need some form of non-linear addition, the simplest form of which is multiplication.  Combing isn't a bad idea.  Neither is a mathematical prism such as FFT.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago in reply to e14 Contributor

    Technically, to be a mixer, in this context, we need some form of non-linear addition, the simplest form of which is multiplication.  Combing isn't a bad idea.  Neither is a mathematical prism such as FFT.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to D_Hersey

    unless it was on a board like a TivaC which has 32*32 multiply built in and plenty of ram image but that would mean switching to TI launch pads so may not be possible in your situation