Arduino
  • Products
  • More
Arduino
Arduino Forum Detect oscillations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 33 replies
  • Answers 1 answer
  • Subscribers 421 subscribers
  • Views 3543 views
  • Users 0 members are here
  • oscillations
  • processing
  • accelerometer
  • movement
  • algorithm
  • arduino
Related

Detect oscillations

kosme
kosme over 12 years ago

I'm trying to use an Arduino and a MMA8452Q accelerometer to sense movement and detect oscillations. What would be the best way to analyze and process the info to detect oscillations at a specific frequency range and act accordingly?

 

Edit 1:


Aswering Michael Kellett questions

Must you detect  a single frequency (known in advance) or a band of frequencies.

I must detect if the oscillation is in the 4-8Hz range.

 

Is the sampling rate under direct contorl of the Arduino or is it set by the accelerometer.

It is mostly under control of the Arduino. The accelerometer is set to sample at a certain rate but I can "miss steps" simply by reading the I2C interface at a much lower rate.

 

What is the range of frequencies and amplitudes you must detect.

I must detect if the oscillation is in the 4-8Hz range. The amplitude will be handled by the accelerometer but I expect it to be between ±4G's

 

Are there other signals present at the same time which you must ignore.

No, but it would be nice to be able to log the results.

 

How quickly must you reach a  decision when the signal appears.

I haven't decided that yet but the oscillation must persist for several seconds before action is taken. The exact number of seconds hasn't still been determined.

 

What accelerometer are you suing.

MMA8452Q I2C accelerometer

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago +1 suggested
    Hello Enrique, It makes it easier for people to follow the thread if you just add a new message rather than editing the original question. It seems that you want to detect energy in the band 4 - 8Hz, not…
  • D_Hersey
    D_Hersey over 12 years ago +1
    SO has just come down with Parky's, so I know of the characteristics of the tremors, they do seem to have a characteristic wave form, narrow fq, fairly constant amplitude between ramp-up and ramp-down…
  • kosme
    0 kosme over 12 years ago in reply to michaelkellett

    I don't have any right now but will get some and post them ASAP

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to kosme

    I'll be interested to have a look at them and see if any ideas come to mind.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago

    Here is a way to translate these requirements into simple code:

    Convert the signal to a rectangular wave.

    • set an upper threshold at half the expected positive peak amplitude
    • set a lower threshold at half the negative peak amplitude
    • this creates a hysteresis where the signal is considered high between a positive threshold crossing and the next negative threshold crossing and it is considered low between a negative threshold crossing and the next positive threshold crossing

    Find periods and amplitudes

    • count the period between positive threshold crossings of the resulting rectangular wave and save each period
    • find the positive peak value between each positive threshold crossing and the next negative threshold crossing and save
    • find the negative peak value between each negative threshold crossing and the next positive threshold crossing and save
    • determine the maximum excursion between positive and negative peaks in each cycle and save
    • now you have numerical periods and amplitudes to analyze for patterns of interest

    Fine tuning

    • If the periods are too short or too long, adjust the thresholds and/or add some pre-filtering
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<