Arduino
  • Products
  • More
Arduino
Arduino Forum wireless display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 1371 views
  • Users 0 members are here
  • led
  • arduino
Related

wireless display

billpenner
billpenner over 12 years ago


I am attempting to build a keypad decoder, a wireless transmitter, a receiver and a 3inch LED display.

The decoder is working but I am having trouble determining what type data to transmit ie. character, byte or integer.

Since I will have to decode the data at the receiver, what would be the best type to use?

The initial code is;

 

#include <Keypad.h>

const byte ROWS = 4; // Four rows
const byte COLS = 3; // Three columns
// Define the Keymap
char keys[ROWS][COLS] = {
  {'1','2','3'},
  {'4','5','6'},
  {'7','8','9'},
  {'#','0','*'}
};

byte rowPins[ROWS] = { 9, 8, 7, 6 }; // keypad rows to Arduino pins

byte colPins[COLS] = { 12, 11, 10 }; //keypad columns to Arduino pins

// Create the Keypad
Keypad kpd = Keypad( makeKeymap(keys), rowPins, colPins, ROWS, COLS );

#define ledpin 13 //define output pin to xmitter

void setup()
{
  
  pinMode(ledpin,OUTPUT);  //for testing
  digitalWrite(ledpin, HIGH); //for testing
  Serial.begin(9600);
}

void loop()
{
   //for (int(c); c <2; c++); I would like to accumulate three bytes and transmit together if possible
   char key = kpd.getKey();
  if(key)  // Check for a valid key.
  {
    switch (key)
    {
      case '#':     //Clear data for re-entry
        digitalWrite(ledpin, HIGH); // for testing
        break;                      // for testing
      case '*':     // Display data on receiver
        digitalWrite(ledpin, LOW);  // for testing
        break;                      // for testing
    
      default:    //send data to xmitter     not working! It only sends to! computer display. 
        Serial.println(key);      // for testing
       

     }
  }  
}

All help would be greatly appreciated. This is a project for our church.

Thanks

Bill

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    If you look at lesson 2 of my tutorials, it deals with reading a character at a time from the serial port into a buffer, a later lesson deals with doing the same from the Ethernet port. The serial port version can easily be adapted to read from the keyboard instead, it then goes on to deal with how to make decisions based on what is read

     

    you can find it here Fast Track to Arduino Programming

     

    the key part in this lesson in your case is replacing the serial.read() with your getkey() and also reducing the buffer size to 3 which you state is your requirements.

     

    You may want to start from lesson 0 though if your not familiar with programming the arduino

     

    If this is still to complicated right now, let me know and I can simplify the relevant parts of the program for you

     

    Regards

     

    peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    If you just want a wireless diplay, you can use a fpv kit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    If you just want a wireless diplay, you can use a fpv kit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billpenner
    0 billpenner over 12 years ago in reply to royston02

    Thanks, but I only need to display a three digit number on a large LED. No video and no quad copters. Thanks tho. I now know what a FPV is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to billpenner

    Then in that case, you can use an xbee/bluethoot module.